12
Entries
Filtered by
'
Communications modules
'
 
Entries per page: 20 50 100
...
1
...
Certificate General Product Approval, China-RoHS, Manufacturer

Statement to China-RoHS directive for SIMATIC ( Panel, ITC, IPC, PG, ET200x, S7-xx, LOGO!, Cables, Network Compontents... ) China-RoHS SIMATIC all V1.5

08/01/2017
ID: 109738555
Product note Product discontinuation for the SIMADYN D closed-loop control system.

Effective October 01, 2015, the manufacture and supply of the SIMADYN D closed-loop control system will be totally discontinued.

03/30/2015
ID: 109475205
Product note End of Production for Certain Components of the SIMADYN D Control System

Effective October 01, 2014 the production and delivery of certain SIMADYN D components will be discontinued. After this date no spare parts will be available anymore and no repairs can be carried out. The complete support of the affected products will be discontinued. ...

07/08/2014
ID: 96999008
FAQ Implementation of SIMATIC modules of the product families S7-300, S7-400, ET 200M, ET 200S ET, 200iSP and TDC in environments with high concentrations of corrosive gas

SIMATIC modules of the product families S7-300 S7-400 ET 200M ET 200S ET 200iSP TDC are also approved for implementation in environments with high concentrations of corrosive gas in compliance with ISA–S71.04 severity level G1; G2; G3. ...

03/26/2013
ID: 28569857
FAQ What should you watch out for in the case of consistent data transfer with SIMOLINK and the expansion module EXM448-1?

Configuration Notes:   In the external cyclic mode (Mode 5) it might happen in the case of a SIMOLINK transfer that, depending on the processing time and order of the SIMOLINK blocks, actual value and setpoint values are transferred in different scan cycles. This happens when the calculation of the blocks in scan time T1 takes longer than the SIMOLINK data transfer.  ...

09/01/2005
ID: 19540984
FAQ How can I improve the stability of a SIMOLINK connection?

Instructions: To reduce the susceptibility to interferences of SIMOLINK connections, it is favourable to ensure permanent telegram traffic. ...

08/22/2005
ID: 21973074
FAQ Using the connector YL on the ramp-function generator block RGJ0F9 (configuration software "STRUC")

QUESTION: What is the purpose of the connector YL on the ramp-function generator block RGJ0F9? ...

12/10/2003
ID: 17823791
Product note Change of the status of some SIMADYN D add-ons

Some SIMADYN D add ons are changed in there status effective at 1.Oct.2002.  For the following SIMADYN D add ons the delivering status is changing on 1.Oct.2002. The components will be in phase-out status and will be regularly available for about one year. After this year the will be only a...

For products: 6DD1688-1AC1
09/24/2002
ID: 13051493
Download PC Software SINEC NML for CSH11

> DESCRIPTION: The PC software (for DOS) SINEC NML and the CSH11 specific supplementary files are required to parameterize the module on the Industrial Ethernet bus. The data set, generated with SINEC NML can be loaded via the RS 232 interface of the CSH11. ...

For products: 6DD1661-0AB1
08/21/2002
ID: 12656760
Manual Base Module CS8 with Communication Board CBP2

Product information

For products: 6SE7090-0XX84-0FF5, 6DD1662-0AC0
10/24/2001
ID: 9126126
Product note Outline of the SIMADYN D components

SIMADYN D is the system which can be used to implement high-dynamic performance technological- and closed-loop drive controls. This graphic, freely-configurable, modular control system using multi-processor technology, processes all of the open- and closed-loop control-, arithmetic- and communica...

09/27/2001
ID: 8765106
Product note Returned equipment of SIMADYN D components

Returned equipment (6DD1.../6DD3... products) must always be send to the following address:...

09/17/2001
ID: 8783186