60
Entries
Filtered by
'
Field PG M2
'
 
Entries per page: 20 50 100
...
1
2
3
...
FAQ How do you enable automatic logon with Microsoft Windows?

When a computer starts up (SIMATIC IPC, for example), you are asked which user name you want to use to log on to the system. This interrupts the automatic startup, which is undesirable, for example, after a power failure.

02/12/2016
ID: 23598260
(3)
FAQ What are the article numbers of the backup batteries for SIMATIC IPCs and SIMATIC Field PGs?

Backup batteries are used to maintain basic functions in the case of a power failure. We explain here how you can determine the article number of the backup battery of your SIMATIC IPC or SIMATIC Field PG.

11/03/2015
ID: 64351747
(3)
Product note Simpler procurement of the AC/DC power supply unit for M2 / M Field PGs

Effective immediately, it is now possible to procure the spare part for the AC/DC power supply unit for field PGs of the M2 / M generation once again without sending in the defective AC/DC power supply unit.

05/28/2015
ID: 109476987
(1)
FAQ What should you watch out for when using Windows XP / Server 2003 on IPCs?

Description Microsoft has announced the end of Extended Support for the operating systems list in Table 01. ...

11/04/2013
ID: 82555422
(0)
FAQ What should you watch out for when restoring a Field PG M4 with Windows 7 from the Restore DVDs supplied?

Description By default the Field PG M4 has two partitions (Drive C: and drive D:). In general drive C: is the system partition and drive D: the data partition on which the project data is stored. When the system is restored, drive C: is restored with the default programs and drive D: is restored as empty. During this procedure the user is requested to assign a user name and password. Windows Setup then installs an administrator account. For example, the user 'pg_user' receives adm ...

10/31/2013
ID: 81784325
(0)
FAQ How does product take back work and which IA and DT products are affected?

Product take back is regulated separately by each member state of the EU. In Germany, the Electrical and Electronics Law (Elektro- und Elektronikgesetz (ElektroG)) of 16.03.2005 regulates this and it is the German implementation of the directives RoHS and WEEE. ...

07/01/2013
ID: 42923229
(1)
FAQ Why can you no longer start the STEP 5 software V7.2/V7.23 after the Windows XP security update KB2707511?

Description Installation of the Microsoft security update KB2707511 for Windows XP can lead to the situation where you can no longer start the STEP 5 software V7.2/V7.23 you have installed. For example, this concerns applications that access device drivers at the Start. STEP 5 is such an application. This security update was published by Microsoft on June 11, 2012. ...

11/12/2012
ID: 62434701
(0)
FAQ What memory expansion options are there for a Field PG?

Field PG P3 / P4 / Celeron / M / M2 / M3 -- Memory expansion for Field PG The Field PGs P3 / P4 / Celeron include a motherboard with two slots for 144-pin SO-DIMM memory modules. The maximum memory expansion for a Field PG P3 is 512MB and for a Field PG P4 1GB. ...

03/22/2012
ID: 21766402
(1)
Download BIOS-Download for Field PG M2

The BIOS updates each contain the changes of the earlier versions listed in the info texts. Please pay careful attention to the following points before or when installing the BIOS update Use the most recent version possible of the BIOS (current release version). Using an older BIOS on a new PC platform can lead to faults. The USB stick or USB disk drive must be the first drive in the boot sequence. Make sure that the power supply is not cut off. Under no circu ...

08/10/2011
ID: 28027230
(2)
Product note BIOS DVD Available for SIMATIC IPCs, PGs and SIMATIC S7-mEC

The BIOS data for the current SIMATIC IPCs, PGs and SIMATIC S7-mEC are now available on a DVD. ...

04/04/2011
ID: 48729827
(0)
Product note Now Available: SIMATIC IPC BIOS-Manager V3.1 (WinPE) for SIMATIC IPCs

The SIMATIC IPC BIOS-Manager V3.1 (WinPE) software, a further development of the proven tool for managing and processing SIMATIC IPC BIOS data, is now available from the Service&Support Internet pages of Industry Automation & Drive Technologies. ...

08/25/2010
ID: 43209333
(0)
FAQ Which software permits you to make a data backup of a running system including the system data partition?

Description Using the SIMATIC IPC Image & Partition Creator V3.x you can make a data backup of a running system including the system partition. The backup procedure might take several hours depending on how loaded the system is, possibly by a WinCC, WinCC flexible or WinAC RTX application. If necessary, the backup file can be split into multiple files. The compression rate can also be selected separately. ...

08/09/2010
ID: 44007853
(0)
Certificate General Product Approval, UL, UL

UL-Approval USA of "Information Technology Equipment" PC, PG, SIMATIC NET, TD, OP (English) Certificate NWGQ.E115352

06/28/2010
ID: 17797670
(0)
Certificate Declaration of Conformity, EC/EU-Declaration of Conformity, Manufacturer

CE Marking (EC-Declaration of Conformity) of the Programming Device Field PG M2 (German/English) Certificate Khe IPC 1-10/2007

For products: 6ES7713-0AA0.-0..., 6ES7713-1BB1.-0...
05/27/2010
ID: 27064636
(0)
Certificate Declaration of Conformity, EC/EU-Declaration of Conformity, Manufacturer

CE Marking (EC-Declaration of Conformity) of the Programming Device Field PG M (German/English) Certificate Khe 1-02/2010

For products: 6ES7713-0AA0.-0..., 6ES7713-1BB1.-0...
04/19/2010
ID: 21953106
(0)
Product note SIMATIC IPC BIOS Manager V3.0 (WinPE) for SIMATIC IPC Now Available

The SIMATIC IPC BIOS Manager V3.0 (WinPE) software, a further development of the proven tool for managing and processing SIMATIC PC BIOS data, is now available for downloading from the Service&Support pages of Industry Automation & Drive Technologies. ...

02/22/2010
ID: 41154009
(0)
Product note SIMATIC Memory Card (SMC) Reader Now Available as Accessory for Field PG M2

The new SMC Card Reader is an optional accessory for the Field PG M2. It has been released for delivery effective Oct. 1, 2009. ...

10/02/2009
ID: 38627741
(0)
Product note SIMATIC Field PG M2 with pre-loaded STEP 7 Basic V10.5 SP1 Software

Updated SIMATIC pre-loaded software Effective October 1, 2009, the Field PG M2 can be ordered with updated SIMATIC software. ...

09/25/2009
ID: 38572895
(0)
Certificate General Product Approval, CCC, CQC

CCC (Certificate for China Compulsary Product Certification) Field PG M2 (Chinese / English) Certificate 2006010902185123

For products: 6ES7713-0AA0.-0..., 6ES7713-1BB1.-0...
08/27/2009
ID: 33973734
(0)
FAQ Where can you obtain a 25-pin to 9-pin adapter (gender changer) for the Field PG, Field PG M and Field PG M2?

Description: You can order the 25-pin to 9-pin adapter from your Siemens sales contact under the following order-no.: A5E00086045 - Serial Port Adapters D9/D25. ...

08/13/2009
ID: 17354655
(1)
 
Entries per page: 20 50 100
...
1
2
3
...