80
Entries
Filtered by
'
Field PG M
'
 
Entries per page: 20 50 100
...
1
2
3
4
...
Application example Connection of an S7 1200 RTU, an S7-1500 and an ET 200SP RTU to a ST7cc central station

With the integration of the SINAUT project planning in the TIA Portal, the complete communication configuration takes place in one tool. The TeleControl portfolio has been expanded with the TIM 1531 IRC, which can be connected to the central control station as a stand-alone device. This means that one or more RTUs can be used as substations in TeleControl systems with the SINAUT ST7 protocol.

04/29/2019
ID: 109761107
(3)
Manual SIMATIC Industrial PC BIOS Description

05/2016, Operating Manual, A5E33664825-AB

06/06/2016
ID: 92189178
(3)
FAQ How do you enable automatic logon with Microsoft Windows?

When a computer starts up (SIMATIC IPC, for example), you are asked which user name you want to use to log on to the system. This interrupts the automatic startup, which is undesirable, for example, after a power failure.

02/12/2016
ID: 23598260
(3)
FAQ What are the article numbers of the backup batteries for SIMATIC IPCs and SIMATIC Field PGs?

Backup batteries are used to maintain basic functions in the case of a power failure. We explain here how you can determine the article number of the backup battery of your SIMATIC IPC or SIMATIC Field PG.

11/03/2015
ID: 64351747
(4)
Product note Simpler procurement of the AC/DC power supply unit for M2 / M Field PGs

Effective immediately, it is now possible to procure the spare part for the AC/DC power supply unit for field PGs of the M2 / M generation once again without sending in the defective AC/DC power supply unit.

05/28/2015
ID: 109476987
(1)
FAQ What should you watch out for with the PPI/MPI/DP interfaces if you want to use the CP 5711 / PC Adapter USB A2 with a SIMATIC S7-200?

System properties of the PPI/MPI/DP interfaces when used with a SIMATIC S7-200.

04/29/2014
ID: 85669627
(6)
FAQ What should you watch out for when using Windows XP / Server 2003 on IPCs?

Description Microsoft has announced the end of Extended Support for the operating systems list in Table 01. ...

11/04/2013
ID: 82555422
(0)
FAQ What should you watch out for when restoring a Field PG M4 with Windows 7 from the Restore DVDs supplied?

Description By default the Field PG M4 has two partitions (Drive C: and drive D:). In general drive C: is the system partition and drive D: the data partition on which the project data is stored. When the system is restored, drive C: is restored with the default programs and drive D: is restored as empty. During this procedure the user is requested to assign a user name and password. Windows Setup then installs an administrator account. For example, the user 'pg_user' receives adm ...

10/31/2013
ID: 81784325
(0)
FAQ How does product take back work and which IA and DT products are affected?

Product take back is regulated separately by each member state of the EU. In Germany, the Electrical and Electronics Law (Elektro- und Elektronikgesetz (ElektroG)) of 16.03.2005 regulates this and it is the German implementation of the directives RoHS and WEEE. ...

07/01/2013
ID: 42923229
(1)
FAQ What memory expansion options are there for a Field PG?

Field PG P3 / P4 / Celeron / M / M2 / M3 -- Memory expansion for Field PG The Field PGs P3 / P4 / Celeron include a motherboard with two slots for 144-pin SO-DIMM memory modules. The maximum memory expansion for a Field PG P3 is 512MB and for a Field PG P4 1GB. ...

03/22/2012
ID: 21766402
(1)
Download BIOS-Download for Field PG M

The BIOS updates each contain the changes of the earlier versions listed in the info texts. Please pay careful attention to the following points before or when installing the BIOS update Use the most recent version possible of the BIOS (current release version). Using an older BIOS on a new PC platform can lead to faults. The USB stick or USB disk drive must be the first drive in the boot sequence. Make sure that the power supply is not cut off. Under n ...

For products: 6ES7712-.....-....
08/10/2011
ID: 23440635
(4)
Certificate General Product Approval, UL, UL

UL-Approval USA of "Information Technology Equipment" PC, PG, SIMATIC NET, TD, OP (English) Certificate NWGQ.E115352

06/28/2010
ID: 17797670
(0)
Certificate General Product Approval, UL, UL

cUL-Approbation Canada for "Information Technology Equipment " PC, PG, SIMATIC NET, TD, OP (English) Certificate NWGQ7.E115352

06/28/2010
ID: 20710247
(0)
FAQ Where can you obtain a 25-pin to 9-pin adapter (gender changer) for the Field PG, Field PG M and Field PG M2?

Description: You can order the 25-pin to 9-pin adapter from your Siemens sales contact under the following order-no.: A5E00086045 - Serial Port Adapters D9/D25. ...

08/13/2009
ID: 17354655
(1)
Application example SIMATIC PC BIOS-Manager V2.204 (for Microsoft Windows)

The 'SIMATIC PC BIOS-Manager' software is available for saving CMOS data and DMI data of SIMATIC PCs. The latest version V2.204 of the BIOS-Manager available here can be used in Microsoft Windows. ...

08/06/2009
ID: 23517919
(0)
FAQ How do you switch the Windows XP MUI and the SIMATIC software to German after delivery of a Field PG?

Instructions: When delivered, the Field PG's operating system, Windows XP MUI, and the SIMATIC software are preinstalled on the hard disk with English menus and dialogs, and a US keyboard layout. The operating system is installed the first time you switch on the Field PG. Even here you can make a number of language settings. ...

05/14/2009
ID: 22309945
(0)
Product note Hard Disk Kit for Field PG M / M2 now with 200 GB S-ATA-HDD

All orders received as from October 01, 2008, for the 'Swappable hard disk' for Field PG M2 will be shipped with a 200-GB S-ATA HDD instead of the previous 160-GB S-ATA HDD. ...

10/21/2008
ID: 31989681
(0)
Product note Field PG M2 Now With CCC Certificate; New Field PG M2 Option "Power Cable for China"

New certificate: As from May 16, 2008, the Field PG M2 is also available with CCC certificate. ...

05/15/2008
ID: 29266635
(0)
FAQ Why doesn't the combo drive of the Field PG work with Windows 2000?

Description: After installing the burner software 'Adaptec Easy CD Creator', the DVD/CD-RW combo drive no longer works properly. In Windows 2000, the DVD/CD-RW combo drive is no longer displayed in the Windows Explorer on the Field PG. The combo drive is displayed with error code 31 in the Device Manager: 'The device is not working properly, because Windows cannot load the drivers needed for the device.' ...

03/25/2008
ID: 14409303
(0)
FAQ Why does the touchpad no longer work after connecting a USB mouse to a Field PG running WIN 2000?

Description: You are using Windows 2000 and have connected a USB mouse. You have selected the driver for the Microsoft Wheel Mouse Optical. In this case the Synaptics touchpad driver is replaced by the Microsoft driver and special functions are lost. Only standard operation is possible. ...

03/12/2008
ID: 11626686
(0)
 
Entries per page: 20 50 100
...
1
2
3
4
...