36
Entries
Filtered by
'
SIMATIC PC FI45 V2
'
 
Entries per page: 20 50 100
...
1
2
...
FAQ How do you download the 3D, CAx and ePLAN data for the SIMATIC products?

You can use the CAx download manager to access the latest product data for your CAD or CAE system.

09/20/2018
ID: 89671877
(3)
FAQ What are the article numbers of the backup batteries for SIMATIC IPCs and SIMATIC Field PGs?

Backup batteries are used to maintain basic functions in the case of a power failure. We explain here how you can determine the article number of the backup battery of your SIMATIC IPC or SIMATIC Field PG.

11/03/2015
ID: 64351747
(3)
FAQ How do you find the UL certificates for SIMATIC modules?

The following instructions show you how to find the UL certificate on our Support pages taking the example of an S7-1500 digital input module (article number: 6ES7 521-1BL00-0AB0).

10/19/2015
ID: 102840331
(3)
FAQ Which program changes have to be made in an S5 controller if a line or graphics operator panel with PROFIBUS connection is replaced by a Windows-based operator panel?

Configuration Notes: If you wish to exchange a line or graphics operator panel, which is connected to a SIMATIC S5 controller via a PROFIBUS DP link, for a Windows-based operator panel, this necessitates the program changes described below. ...

11/27/2009
ID: 31676209
(0)
FAQ Which PCI slots in the SIMATIC PCs have exclusive use of the interrupt - i.e. don't share it with other PCI devices?

Configuration notes: Overview of PCI slots without interrupt sharing In the example below we show the assignments of the PCI IRQ lines to the PCI slots of Rack PC 847B. Modules requiring an exclusive interrupt can be used for slot 5 or 8 and 6 or 9 in the APIC mode. ...

08/18/2008
ID: 12981782
(0)
FAQ How can you calculate the actual local time (summer time or winter time) in the S7-300/400 CPU and then use it on the panel as system time?

There is no time conversion of the S7-300/400 CPU clock to summer or winter time in automation facilities with integrated time synchronization.

08/15/2008
ID: 19324378
(0)
FAQ How can you influence the assignment of interrupts with SIMATIC PCs and check the assignment of resources in the system information in Windows 2000/XP?

Influencing the assignment of interrupt with SIMATIC PCs The table below explains how you can manually influence the assignment of interrupts in the BIOS Setup with SIMATIC RACK PC 840, BOX PC 840, BOX PC 620, Panel PC 870 and Panel PC 670. The changes made here also affect the assignment of interrupts in the Windows operating system. ...

01/03/2006
ID: 21498129
(0)
Product note Discontinuation of Manufacture: Panel PC FI45 V2

The Panel PC FI45 V2 has been discontinued since 09/30/2003. Orders received by 09/30/2003 will be delivered by 12/31/2003 at the latest. There is still a non-binding possibility that a few devices will be manufactured until 12/31/2003. ...

For products: 6ES7645-3....-....
01/20/2004
ID: 17583074
(0)
Certificate Declaration of Conformity, EC/EU-Declaration of Conformity, Manufacturer

CE Marking (EC-Declaration of Conformity) of SIMATIC (English/German) Certificate

07/29/2003
ID: 16671315
(0)
Product note Marketing Announcement: Phase-Out Planning Panel PC FI45 V2 -  final Order Opportunity!  

The manufacture of the Panel PC FI45 V2 will be stopped as planned at the end of the 02/03 fiscal year.   The final orders will be accepted on 09/30/2003. ...

For products: 6ES7645-3....-....
06/10/2003
ID: 15257455
(0)
FAQ Exchange of background illumination in SIMATIC FI45

QUESTION: How can I renew the background illumination of the FI45 display? ANSWER:...

For products: 6ES7645-3....-...., 6ES7645-2....-....
12/16/2002
ID: 13983531
(0)
FAQ Where do you find the slot number of a PCI slot in a SIMATIC PC?

Description:   The following table shows position and sequence of PCI slots for current SIMATIC PCs. Normally, the assignments can be found in the manual for each SIMATIC PC or imprinted on the motherboard next to the PCI slots.  ...

11/15/2002
ID: 13589353
(0)
Product note FI45/WinCC: Added to the Discontinued Items Catalog; planned Phase Out

The ready-to-use WinCC system based on the FI45 will no longer be updated and thus has been added to the discontinued items catalog. The discontinuation phase will be shortened significantly, since the FI45 as well as WinCC are available separately for replacement purposes.   ...

08/01/2002
ID: 12351384
(0)
Product note Discontinuation Planning: FI45

With the complete availability of the Panel PC spectrum consisting of the PC670, PC870 and IL70, the migration phase of FI45 customers to the new product spectrum has begun. ...

08/01/2002
ID: 12370028
(0)
Product note FI45 V2 Product Cancellation: 400 MHz Celeron and 500 MHz Pentium III Versions Delivery Release: 450/700 MHz Pentium III, Win2000

The versions with 400 MHz Celeron and 500 MHz Pentium III processors are replaced by versions with 450 MHz Pentium III and 700 MHz Pentium III processors. The hard drive now has a capacity of 10.2 GB. The operating system Windows 2000 can now be selected. The list prices have been adjusted accord...

10/10/2000
ID: 5117019
(0)
Product note Industrial PC - Debugging in the SOM Safecard Driver

A new, debugged SOM driver(Safecard On Motherboard) is available with immediate effect for all SIMATIC PCs based on the Intel Celeron or Pentium III. This new driver should be used with immediate effect to avoid possible PC malfunctioning. The following order nu ...

07/06/2000
ID: 4558381
(0)
Product note SIMATIC PC FI45 V2; Protective Film

A protective plastic film for the SIMATIC PC FI45 V2 has been released with immediate effect. A self-adhesive protective film is offered with immediate effect to protect the SIMATIC PC F145 V2 (particularly the touch screen versions) from mechani ...

06/07/2000
ID: 4558280
(0)
Product note SIMATIC PC FI45 V2

SIMATIC PC FI45 V2: the F145 product series is being revamped. The existing SIMATIC F145s are to be replaced by the improved FI45 Version 2 models. The new versions are available immediately. _1. Product Descriptio ...

03/29/2000
ID: 4297607
(0)
Download Keyboard driver and device-specific ProTool add-on

DESCRIPTION: The attached self-extracting file contains the German keyboard driver for FI25 and FI45. It also contains the add-on files for the device-specific layouts for configuring with ProTool/Pro as well as the corresponding entries required for the ProTool.ini. ...

11/22/1999
ID: 1435676
(0)
Product note SIMATIC PC FI45 New standard equipment processor

_1. General Information_ The standard SIMATIC PC FI45 variant has been given (delivery direct from stock) a 333MHz Intel Pentium II processor. This model supersedes the previous standard processor, a 266MHz Intel Pentium II. The 333MHz Intel Pentium II processor also supersedes the 26 ...

10/19/1999
ID: 4296685
(0)
 
Entries per page: 20 50 100
...
1
2