×
Siemens Industry Online Support
Siemens AG
Filter criteria for entries
All Products
My Products
Product tree
 
 
Clear all filters
Product
Search product
Entry type
 
Date
Task
  • Save filter
  • Load filter
  • email on update
643
Entries
Filtered by
'
PROFIBUS
'
and
'
FAQ
'
 
Entries per page: 20 50 100
...
1
2
3
4
5
...
FAQ How do you use SIMATIC NET modules in IPC 427D and IPC 427E taking into account the maximum permissible power loss?

Due to thermal restrictions, the power loss is restricted to a maximum of 5W per slot for the versions of IPC 427D and IPC 427E with one or two PCIe slots.

09/17/2019
ID: 109770863
FAQ How do you use SIMATIC NET PC modules in IPC 277D and IPC 277E taking into account the maximum permissible power loss?

Due to thermal restrictions, the power loss is restricted to a maximum of 5W for the versions of IPC 277D and IPC 277E with a PCIe slot.

09/17/2019
ID: 109770855
FAQ Compatibility Tool for Automation and Drive Technology

The Compatibility Tool is a function provided by the Industry Online Support with which you can select compatible software products or check the compatibility of existing configurations.

09/03/2019
ID: 64847781
FAQ Which modules support the "S7 Routing" function in S7 subnets?

This entry shows which modules support the "S7 Routing" function in S7 subnets to be able to operate cross-network PG/OP communication through S7 Routing.

08/01/2019
ID: 584459
FAQ How should you proceed if installation of the SIMATIC NET PC software is not completed successfully?

Installation of the SIMATIC NET PC software is not completed successfully

07/22/2019
ID: 19809395
FAQ How do you connect the RS485/RS422 interfaces of SIMATIC and SIPLUS modules for serial communication?

Serial communication is possible via the RS485 and RS422 interfaces with the modules below, . The terminal assignments are given in the diagrams.

04/23/2019
ID: 109736665
FAQ What are the quantity frameworks and performance data of each of the SIMATIC NET products?

Quantity frameworks and performance data of the SIMATIC NET products

04/09/2019
ID: 15227599
FAQ Which user authorizations do you need to be able to collect hardware information with the SAS-DC (SIMATIC Assessment Suite - Data Collector)?

Read out device and diagnostics information

02/14/2019
ID: 109763454
FAQ How do you efficiently collect diagnostics and system information with the SIMATIC Assessment Suite - Data Collector (SAS-DC)?

The SIMATIC Assessment Suite - Data Collector (SAS-DC) - formerly known as SIMATIC Diagnostics Tool (SDT) - enables you to simply and easily collect diagnostics and system information from computers or other devices.

01/22/2019
ID: 65976201
FAQ How do you fasten the PROFIBUS bus connector.

To connect PROFIBUS cables there are bus connectors with cut-and-clamp technology for FastConnect systems and with screw terminals.

11/30/2018
ID: 109760665
FAQ What do you have to do if, after adding a CP or an FM module, the SIMATIC S7-300 CPU no longer switches to RUN mode?

After adding a CP or an FM module, the SIMATIC S7-300 CPU no longer switches to RUN mode but remains in STOP mode.

10/19/2018
ID: 22410800
FAQ Diagnostic coverage level to be specified and achievable safety integrity level for subsystems or SRP/CS with electromechanical components

This entry provides information on the diagnostic coverage level.

09/28/2018
ID: 35444114
FAQ Which USB-MPI adapter can be used for the maintenance and commissioning of the SINUMERIK 810D/840D and what should you watch out for here?

There are differences between the MPI interface of the SINUMERIK 810D/840D and the MPI interface of the SIMATIC. The main difference is that there is no 24V power supply in the MPI interface of the SINUMERIK.

For products: 6GK1571-1AA00
09/20/2018
ID: 109759156
FAQ How do you download the 3D, CAx and ePLAN data for the SIMATIC products?

You can use the CAx download manager to access the latest product data for your CAD or CAE system.

09/20/2018
ID: 89671877
FAQ Information about manuals on the topic of "CPU and CP Compatibility"

In an automation system, a communication processor (CP) can only be operated with a CPU. In the system test, the relevant CPUs are tested with the separate Ethernet CPs and released accordingly.

08/03/2018
ID: 26561772
FAQ How do you use the PROFIBUS optical cables for PROFINET?

When exchanging the interface modules between electrical and optical transmission you can use the existing PROFIBUS fiber optic cables also with PROFINET.

04/19/2018
ID: 109754843
FAQ Which licenses can you use for new SIMATIC NET PC software?

Up to and including the SIMATIC NET CD Edition 2005+HF1 (V6.3) it was possible to order the SIMATIC NET CD separately as an upgrade without the SIMATC NET license key in order to upgrade the SIMATIC NET PC software. Here, old SIMATIC NET license keys were accepted by new SIMATIC NET PC software, so that they could continue to be used.

04/10/2018
ID: 22090049
FAQ Sirius ACT Sensor Buttons in Two-Hand Control Station

This FAQ describe how can a two-hand control station including sensor buttons 3SU1 get the IEC62061 (SIL3), respectively ISO13849-1 (PL e).

03/05/2018
ID: 109479531
FAQ How do you insert a C-PLUG or what is the purpose of a C-PLUG?

The C-PLUG (configuration plug) is an interchangeable medium on which the configuration data of a device is automatically saved. This enables you to exchange a defective module simply by replugging the C-PLUG to a new module.

02/14/2018
ID: 24030688
FAQ How do you program the communication blocks FC50 and FC60?

To communicate using one of the following communication connections you must call the communication blocks FC50 "AG_LSEND" and FC60 "AG_LRECV" in the user program of the S7-400 CPU.

01/18/2018
ID: 18513371
 
Entries per page: 20 50 100
...
1
2
3
4
5
...