×
Siemens Industry Online Support
Siemens AG
Filter criteria for entries
Product tree
 
 
Clear all filters
Product
Search product
Entry type
 
Date
Task
  • Save filter
  • Load filter
  • email on update
17
Entries
Filtered by
'
Bus terminals
'
and
'
FAQ
'
 
Entries per page: 20 50 100
...
1
...
FAQ Which components do you use to terminate PROFIBUS subnets with a terminator?

Description With PROFIBUS, each bus segment must be terminated at both ends with a terminator. The line termination consists of a resistor combination. This is integrated in the RS 485 Repeater, in the OLM (channel 2), in the bus terminal, in the active RS 485 terminating element and in some bus connectors. If these components are used at the end of a segment, then the terminator must be activated. ...

12/08/2014
ID: 187276
FAQ How do you define the assignment of the MPI/DP interface?

Description The assignment of the MPI/DP interface is as follows. Fig. 1: Connector assignment...

11/23/2010
ID: 3001321
FAQ How do you connect a SIEMENS POWER MONITOR (SIMEAS P) to SIMATIC S7?

Instructions: You can connect a SIEMENS POWER MONITOR (SIMEAS P) to a SIMATIC S7-300/S7-400 via PROFIBUS-DP. ...

12/17/2007
ID: 16626821
FAQ What alternatives are there to connecting to the multimaster network on the PC side?

Configuration Notes: To incorporate the PC station in the multimaster network communication can be made via RS-232/PPI multimaster cable (6ES7901-3CB30-0XA0) USB/PPI multimaster cable (6ES7901-3DB30-0XA0) PC Adapter USB (6ES7972-0CB20-0XA0) ...

07/17/2007
ID: 22634774
FAQ Which network configuration is typical when implementing the multimaster function?

Configuration Notes: The following figure shows an example of a multimaster network with multiple masters and one slave. ...

07/02/2007
ID: 22635121
FAQ How do you set up a redundant optical ring with two OLMs and what LED display behavior is to be expected?

This entry shows you how to set up a redundant optical ring with two OLMs and what LED display behavior is to be expected.

02/13/2006
ID: 22561265
FAQ Why is the Diagnostics Repeater recognized in "Accessible Nodes", but not in the Online Hardware?

  Description: A PROFIBUS with Diagnostics Repeater is connected to an S7-300 station (CPU 315-2 DP) via a CP 342-5. ...

01/03/2006
ID: 22404586
FAQ How do you set the terminators on the Diagnostics Repeater for the different interfaces?

  Description: For the different interfaces you select the settings as given in the table below. ...

01/03/2006
ID: 22410028
FAQ How do you set up a redundant optical ring with PROFIBUS OLMs?

Instructions:   The diagram below shows how to set up a redundant optical ring with PROFIBUS OLMs: ...

11/30/2005
ID: 19758281
FAQ Commissioning a non-functioning DP master system

QUESTION:   How can I commission a non-functioning DP master system?  ANSWER:...

09/01/2004
ID: 19379085
FAQ Diagnostics tools for commissioning the PROFIBUS DP network

QUESTION: What options to I have for diagnosing errors in the DP master system during the commissioning phase?  ...

09/01/2004
ID: 19378851
FAQ No online connection with STEP 7 after closing Amprolyzer

QUESTION:   Why can't I set up any more online connections with STEP 7 or why is it no longer possible to access the internal prommer interface after closing the Amprolyzer? ...

08/20/2004
ID: 19345841
FAQ Power Supplies Suitable for PROFIBUS OLM

QUESTION: What do I have to observe, if I want to connect a power supply to a PROFIBUS OLM? ...

07/28/2004
ID: 19255979
FAQ Taking repeaters into account in the hardware configuration

QUESTION: Do I have to take the implementation of repeaters into account in my hardware configuration? ...

11/19/2003
ID: 17638231
FAQ Report "MS Excel is required" while opening the Amprolyzer

QUESTION: Why does the report 'MS Excel is required' appear if I open the Amprolyzer? ...

10/29/2003
ID: 17452627
FAQ Operating modules with the diagnostics repeater (6ES7 972-0AB00-0XA0, 6ES7 972-0AB01-0XA0)

QUESTION:  - ANSWER: The following table contains a list of modules that have been tested and measured during the development of the diagnostics repeater (6ES7 972-0AB00-0XA0, 6ES7 972-0AB01-0XA0). You can use this table to determine compatibility with the diagnostics repeater. ...

08/11/2003
ID: 16704567
FAQ Using a diagnostics repeater on an external master

QUESTION: Can I use the diagnostics repeater also on an external master? ANSWER:...

07/14/2003
ID: 16502503