28
Entries
Filtered by
'
TIM 4R / 4RD (for S7-300/-400/PC)
'
 
Entries per page: 20 50 100
...
1
2
...
Certificate General Product Approval, China-RoHS, Manufacturer

Statement on the China RoHS directive, SIMATIC NET

10/12/2018
ID: 109738732
(2)
Manual SIMATIC NET: Glossary - Specialist terms

11/2017, Reference Manual, C79000-G8976-C259-07

12/12/2017
ID: 50305045
(3)
Certificate General Product Approval, Manufacturer Declaration, Manufacturer

CCC Statement regarding the CCC certificate -

11/16/2016
ID: 109743044
(2)
Certificate EMC, KC

KCC Registration of Broadcasting and Communication Equipments Korea for SINAUT ST7 KCC-REM-S49-TELECONTROL

06/17/2015
ID: 59534823
(0)
Product note Type Discontinuation of TIM Modules TIM 4R and TIM 4RD

Effective April 15, 2015, the TIM modules TIM 4R and TIM 4R D will be given the product status “Product Cancellation“.

04/13/2015
ID: 109475169
(0)
Catalog/Brochure Catalog IK PI - Industrial Communication SIMATIC NET

2015, Catalog, E86060-K6710-A101-B8-7600, E86060-K6710-A101-B8-7600

03/12/2015
ID: 109745642
(0)
Catalog/Brochure Katalog IK PI - 2015, Kap. 7: Industrial Remote Communication

Catalog

03/05/2015
ID: 109765556
(0)
Product note Phase out declaration TIM modules TIM 4R and TIM 4RD

  The TIM modules TIM 4R and TIM 4R D will be set to the product status 'phase out' with effect from October 01, 2014. ...

09/01/2014
ID: 100698750
(0)
Product note Conversion from GSM-CSD services by Deutsche Telekom (T-Mobile)

Deutsche Telekom will convert the CSD service in GSM networks to IP technology. This affects all systems that utilize this service, in particular it affects the data transmission in SINAUT ST1 and ST7 systems. ...

01/25/2011
ID: 48034649
(0)
Manual SINAUT ST7 System Manual Volume 1: System and Hardware

05/2007, Operating instructions, C79000-G8976-C178-6

09/24/2009
ID: 24621696
(0)
Manual SIMATIC NET: SINAUT ST7 Software Volume 2: Software

05/2007, System Manual, C79000-G8976-C222-06

09/24/2009
ID: 24619519
(0)
Product note Provision of Analog Standard Fixed Telephone Lines from Deutsche Telekom to Be Discontinued

Not later than September 30, 2009 Deutsche Telekom will disconnect all analog standard fixed telephone lines, also known as “analog dedicated lines“ or “leased lines“. This will affect SINAUT systems which are connected via such lines with modems. ...

09/08/2008
ID: 30374438
(0)
FAQ What are the causes and remedies for some of the CPU error messages in SINAUT ST7?

Description: The following provides a detailed description of causes and remedies for some of the CPU error messages. ...

06/18/2008
ID: 29585871
(0)
FAQ Which CPUs can you use together with SINAUT ST7?

Configuration notes: In principle, you can use any SIMATIC S7-CPU (S7-300, S7-400, C7 complete device) in the SINAUT ST7 system. There is the SINAUT MICRO solution for S7-200. There is further information on this in the application in Entry ID: 22537809 ...

02/07/2008
ID: 24059469
(0)
FAQ How do you configure time synchronization in a SINAUT network?

Instructions: In the SINAUT ST7 system it is possible to have a uniform time synchronization of all SINAUT nodes. This gives the process data a unique time stamp. In the case of stations that are connected via a dial-up network, you can also use the time synchronization to regularly check the availability of these stations and retrieve the data stored there during synchronization. ...

01/07/2008
ID: 23810539
(0)
FAQ How can you block the polling of individual stations in a SINAUT dedicated line network?

Instructions: If dedicated-line subscribers are to be added to a SINAUT project, which were not all available when the plant was commissioned, then calling the stations leads to a higher polling cycle, because the missing stations do not yet respond to the call through the central TIM. ...

11/21/2006
ID: 24072753
(0)
FAQ Which special services have to be set for sending text messages in a SINAUT project?

  Configuration notes: SMS special services are selected depending upon the provider and the type of network access, so as to enable text messages to be sent via the interface set. ...

10/18/2006
ID: 24045718
(0)
FAQ Why does the status of a TIM not appear with the SINAUT diagnostics tool when you use the ST1 protocol?

  Description: The TIM node diagnostics can be called for a TIM using the SINAUT diagnostics and service tool The current statuses of all the SINAUT nodes which are connected to the TIM are displayed in the diagnostic window. ...

10/18/2006
ID: 24044216
(0)
FAQ Which settings have to be defined in order to send text messages (SMS) to a fax machine using SINAUT ST7?

  Configuration notes: If you wish to send a text message to a fax machine and not, as would ordinarily be the case, to another mobile phone user, specify the provider's gateway number followed by the recipient's fax number in the 'SMS DB configuration' of the SINAUT configuration tool instead of the mobile phone number. ...

10/18/2006
ID: 24043847
(0)
FAQ What options exist for doing a test without modems using a zero modem cable?

  Configuration notes: You can make a direct connection between two TIM modules without a modem using a zero modem cable. ...

10/18/2006
ID: 23806944
(0)
 
Entries per page: 20 50 100
...
1
2
...