×
Siemens Industry Online Support
Siemens AG
Filter criteria for entries
All Products
My Products
Product tree
 
 
Clear all filters
Product
Search product
Entry type
 
Date
Task
  • Save filter
  • Load filter
  • email on update
16
Entries
Filtered by
'
TIM 4R / 4RD (for S7-300/-400/PC)
'
and
'
FAQ
'
 
Entries per page: 20 50 100
...
1
...
FAQ What are the causes and remedies for some of the CPU error messages in SINAUT ST7?

Description: The following provides a detailed description of causes and remedies for some of the CPU error messages. ...

06/18/2008
ID: 29585871
(0)
FAQ Which CPUs can you use together with SINAUT ST7?

Configuration notes: In principle, you can use any SIMATIC S7-CPU (S7-300, S7-400, C7 complete device) in the SINAUT ST7 system. There is the SINAUT MICRO solution for S7-200. There is further information on this in the application in Entry ID: 22537809 ...

02/07/2008
ID: 24059469
(0)
FAQ How do you configure time synchronization in a SINAUT network?

Instructions: In the SINAUT ST7 system it is possible to have a uniform time synchronization of all SINAUT nodes. This gives the process data a unique time stamp. In the case of stations that are connected via a dial-up network, you can also use the time synchronization to regularly check the availability of these stations and retrieve the data stored there during synchronization. ...

01/07/2008
ID: 23810539
(0)
FAQ How can you block the polling of individual stations in a SINAUT dedicated line network?

Instructions: If dedicated-line subscribers are to be added to a SINAUT project, which were not all available when the plant was commissioned, then calling the stations leads to a higher polling cycle, because the missing stations do not yet respond to the call through the central TIM. ...

11/21/2006
ID: 24072753
(0)
FAQ What options exist for doing a test without modems using a zero modem cable?

  Configuration notes: You can make a direct connection between two TIM modules without a modem using a zero modem cable. ...

10/18/2006
ID: 23806944
(0)
FAQ Which special services have to be set for sending text messages in a SINAUT project?

  Configuration notes: SMS special services are selected depending upon the provider and the type of network access, so as to enable text messages to be sent via the interface set. ...

10/18/2006
ID: 24045718
(0)
FAQ Which settings have to be defined in order to send text messages (SMS) to a fax machine using SINAUT ST7?

  Configuration notes: If you wish to send a text message to a fax machine and not, as would ordinarily be the case, to another mobile phone user, specify the provider's gateway number followed by the recipient's fax number in the 'SMS DB configuration' of the SINAUT configuration tool instead of the mobile phone number. ...

10/18/2006
ID: 24043847
(0)
FAQ Why does the status of a TIM not appear with the SINAUT diagnostics tool when you use the ST1 protocol?

  Description: The TIM node diagnostics can be called for a TIM using the SINAUT diagnostics and service tool The current statuses of all the SINAUT nodes which are connected to the TIM are displayed in the diagnostic window. ...

10/18/2006
ID: 24044216
(0)
FAQ Which control systems have been successfully used with the SINAUT ST7?

  Configuration notes: The following control systems have been successfully used in conjunction with the SINAUT ST7. ...

10/18/2006
ID: 24044826
(0)
FAQ Which settings have to be defined in order to send text messages (SMS) to an e-mail recipient using SINAUT ST7?

  Configuration notes: If you wish to send a text message to an e-mail address and not, as would ordinarily be the case, to another mobile phone user, the text message starts with the recipient's e-mail address, following by the actual text. ...

10/13/2006
ID: 24039110
(0)
FAQ MPI coupling from SINAUT ST7 TIM to SIMATIC STEP7 CPU400

QUESTION: How many SINAUT ST7 TIM modules can be operated on a SIMATIC S7 CPU400? ...

11/16/2004
ID: 19758408
(0)
FAQ MPI coupling from SINAUT ST7 TIM to SIMATIC NET CP5613

QUESTION: How many SINAUT ST7 TIM modules can I operate on a SIMATIC NET CP5613? ...

11/16/2004
ID: 19758635
(0)
FAQ SINAUT ST7 TIM in the expansion rack

QUESTION: Which SIMATIC S7 IM modules do I need to use in order to operate a SINAUT ST7 TIM in the expansion rack of an S7-300 station? ...

11/16/2004
ID: 19757971
(0)
FAQ DCF77 time-of-day signal via a GPS kit

QUESTION: How can I send the requisite time signal to a TIM with a DCF77 receiver if the signal cannot be received from Frankfurt am Main (Germany).  ...

11/16/2004
ID: 19760480
(0)
FAQ MPI coupling from SINAUT ST7 TIM to SIMATIC NET CP5611

QUESTION: How many SINAUT ST7 TIM modules can be operated on a SIMATIC NET CP5611? ...

11/16/2004
ID: 19760705
(0)
FAQ MPI coupling from SINAUT ST7 TIM to SIMATIC S7 CPU300

QUESTION: How many SINAUT ST7 TIM modules can be operated on a SIMATIC S7 CPU300? ...

11/05/2004
ID: 19741461
(0)
 
Entries per page: 20 50 100
...
1
...