25
Entries
Filtered by
'
UMTS-Router SCALANCE M873
'
 
Entries per page: 20 50 100
...
1
2
...
Application example SIMATIC S7-based Telecontrol via DNP3 Protocol

The control station communicates with the outstations via Ethernet using the DNP3 telecontrol protocol.

05/16/2019
ID: 87447188
(3)
Product note  Elimination of yellow inspection stickers on SCALANCE modules

 Elimination of yellow inspection stickers on SCALANCE modules

04/09/2019
ID: 109766528
(0)
Certificate General Product Approval, China-RoHS, Manufacturer

Statement on the China RoHS directive, SIMATIC NET

10/12/2018
ID: 109738732
(2)
Manual SIMATIC NET: Glossary - Specialist terms

11/2017, Reference Manual, C79000-G8976-C259-07

12/12/2017
ID: 50305045
(3)
Manual SIMARIS Software SIMARIS therm Planning Tool

11/2016, Operating Manual

03/06/2017
ID: 109744553
(5)
FAQ Which security modules support the dynamic DNS function (DDNS)?

Using DDNS you can access a module with dynamic IP address via a Fully Qualified Domain Name (FQDN) defined with a specific provider (own).

01/27/2017
ID: 62812011
(1)
Product note Announcement of "Product phase-out“ UMTS-Router SCALANCE M873

The UMTS Router SCALANCE M873 will be set to the status "Product phase-out" with effect from 31 July 2016.

For products: 6GK5873-0AA10-1AA2
07/25/2016
ID: 109739377
(0)
Application example Sending and Receiving SMS Messages via a SCALANCE M Router

A SIMATIC S7-1200/1500 station is to automatically send important information about the plant status, alarm messages or warnings to mobile service personnel using the SCALANCE M874/M876 router.

06/15/2016
ID: 54361177
(11)
Download Power loss data for control panel devices

This is a list with power loss data for many components for a control panel

04/27/2016
ID: 109480404
(15)
Application example Setting up a secure VPN Connection between SCALANCE M-800 and SSC Using a static IP Address

Establish a secure connection between a service technician and an automation cell over the Internet with the aid of the SOFTNET Security Client and a SCALANCE M-800.

12/10/2015
ID: 109481101
(1)
Certificate Radio Equipment Type Approval Certificate,

Overview Countries radio approvals for TS MODULE GSM und Scalance M873

For products: 6GK5873-0AA10-1AA2, 6GK7972-0MG00-0XA0
05/15/2015
ID: 49312810
(0)
Application example Setting up a secure VPN Connection between CP x43-1 Advanced and M874 Using a static IP Address

This application shows how to establish a secure connection between two networks over the Internet with the aid of CP x43-1 Advanced and M874.

04/28/2015
ID: 108913753
(2)
Catalog/Brochure Catalog IK PI - Industrial Communication SIMATIC NET

2015, Catalog, E86060-K6710-A101-B8-7600, E86060-K6710-A101-B8-7600

03/12/2015
ID: 109745642
(0)
Certificate Declaration of Conformity, RCM, ACMA

RCM (C-Tick), ACMA, Supplier's Declaration of Conformity Australia for Industrial Communication and Identification ABN 98 004 347 880

03/06/2015
ID: 103880810
(0)
Catalog/Brochure Katalog IK PI - 2015, Kap. 7: Industrial Remote Communication

Catalog

03/05/2015
ID: 109765556
(0)
Application example Setting up a secure VPN Connection between SCALANCE S and M874 Using a static IP Address

Task Due to increased networking through Ethernet, remote diagnostics and/or remote maintenance are of great importance in modern automation systems. Today's Internet access mechanisms (wireless, broadband) and the security components from Siemens are an ideal combination for industrial remote co...

10/29/2014
ID: 99681225
(0)
Application example Setting up a secure VPN Connection between SCALANCE S and M812-1 Using a static IP Address

Task Due to increased networking through Ethernet, remote diagnostics and/or remote maintenance are of great importance in modern automation systems. Today's Internet access mechanisms (wireless, broadband) and the security components from Siemens are an ideal combination for industrial remote co...

10/21/2014
ID: 99681595
(0)
FAQ In which country is my mobile telephone device (GSM/EDGE/UMTS/LTE) approved?

The current list of mobile telephone approvals is available at the link below.

05/21/2014
ID: 91438171
(0)
FAQ How do you code an SMS text in the GSM 3.38 cellular radio standard?

Description If you use the S7 CPU to send an SMS message over the cellular phone network, you must observe the following for the coding of the SMS text. ...

04/01/2014
ID: 67395899
(0)
Product note Delivery Release of the New Firmware V1.316 for MD741-1 EGPRS ROUTER and SCALANCE M873 UMTS ROUTER

The new firmware version 1.316 is now available for the MD741-1 (EGPRS) and SCALANCE M873 (UMTS) mobile radio routers. Existing products in the field with the earlier firmware version can be updated with a firmware update. ...

For products: 6GK5873-0AA10-1AA2, 6NH9741-1AA00
02/03/2014
ID: 87559169
(0)
 
Entries per page: 20 50 100
...
1
2
...