21
Entries
Filtered by
'
MD3 Telephone Modem
'
 
Entries per page: 20 50 100
...
1
2
...
Manual SIMATIC NET: Glossary - Specialist terms

09/2021, Reference Manual, C79000-G8976-C259-08

09/24/2021
ID: 50305045
(4)
Product note SITRAIN course: Remote Communication in Industrial Networks (IK-REMOTES)

11/09/2020
ID: 109784064
(0)
Product note White paper "Cybersecurity for Telecontrol for Water and Wastewater Industry", edition 06/2020

The updated white paper "Cybersecurity for Telecontrol for Water and Wastewater Industry" was published in June 2020.

07/09/2020
ID: 109780795
(0)
Certificate General Product Approval, China-RoHS, Manufacturer

Statement on the China RoHS directive, SIMATIC NET

10/12/2018
ID: 109738732
(2)
Manual SIMARIS Software SIMARIS therm Planning Tool

11/2016, Operating Manual

03/06/2017
ID: 109744553
(15)
Certificate General Product Approval, Manufacturer Declaration, Manufacturer

CCC Statement regarding the CCC certificate -

11/16/2016
ID: 109743044
(2)
Product note Discontinuation of SINAUT MD3 dial-up modem

As announced on 14 March 2016, the SINAUT MD3 analog dial-up modem will be set to the product status "discontinuation" with effect from 1 October 2016.

For products: 6NH7810-0AA30
08/15/2016
ID: 109740148
(0)
Certificate Declaration of Conformity, EC/EU-Declaration of Conformity, Manufacturer

EU-Declaration of Conformity for SINAUT ST?, MD2 and MD3 PD-PA-Cl-PLC-0A4-160126

For products: 6NH7810-0AA30, 6NH7810-0AA20
02/19/2016
ID: 109482924
(0)
Certificate Declaration of Conformity, EC/EU-Declaration of Conformity, Manufacturer

EU Declaration of Conformity for SIMATIC TC, SINAUT ST7 MD2 und MD3 PD-PA-Cl-PLC-0A4-160126

For products: 6NH7810-0AA30, 6NH7810-0AA20
02/03/2016
ID: 109482507
(0)
Catalog/Brochure Katalog IK PI - 2015, Kap. 7: Industrial Remote Communication

Catalog

03/05/2015
ID: 109765556
(0)
Certificate Declaration of Conformity, EC/EU-Declaration of Conformity, Manufacturer

EC Declaration of Conformity for SIMATIC TC, SINAUT ST7 SC_Cl_I0713-83

07/16/2013
ID: 77320868
(0)
FAQ What should you watch out for when selecting a modem for use with SIMATIC S7 TeleService?

Description For SIMATIC TeleService you need one modem on the Service PG/PC and under circumstances one modem on the TS Adapter on the remote plant. The latest TS Adapter versions have an integrated modem (as from TS Adapter II), but for special cases also allow you to connect an external modem via an RS232 serial interface. ...

06/11/2013
ID: 1096710
(0)
Product note List Price Increase for Several SINAUT Products

Due to a general increase in costs, the list prices of a number of SINAUT products will be increased effective October 01, 2012. ...

06/18/2012
ID: 61481580
(0)
Product note Conversion from GSM-CSD services by Deutsche Telekom (T-Mobile)

Deutsche Telekom will convert the CSD service in GSM networks to IP technology. This affects all systems that utilize this service, in particular it affects the data transmission in SINAUT ST1 and ST7 systems. ...

01/25/2011
ID: 48034649
(0)
Product note Delivery stop revovement

With immediate effect, the delivery stop introduced on 30 March 2010 for the modules listed here, due to the missing CE update and R&TT approval, is to be lifted again. The applicable tests have been passed in accordance with the current guidelines for achieving CE certification. Any suppleme...

06/29/2010
ID: 43385536
(0)
FAQ How do you protect a SINAUT MD3 dial-up network modem against overvoltage?

Configuration Notes: The modem has an overvoltage protection between the two signal lines 'a' and 'b'. Overvoltage to protective ground is dangerous for the modem, because it always takes the path of least resistance. ...

For products: 6NH7810-0AA30
10/23/2008
ID: 31938455
(0)
FAQ How can you send a text message (SMS) with SINAUT ST7?

Description: It is possible to send an SMS from the GSM network or from the landline network. This description is valid for the GSM network. If you are using a landline network in your configuration, follow the Notes at the end of this entry. ...

For products: 6NH7810-0AA40, 6NH7810-0AA30, 6NH9720-3AA00
10/13/2008
ID: 31912114
(0)
FAQ Which modem replaces the MD125 modem?

Configuration Notes: The MD3 dial-up modem (6NH7810-0AA30, hardware release > 4) can be used to replace the MD125 dial-up modem (6NH9810-2T). The MD3 is compatible with the MD125 only in the following operating modes: 1200 bps dx (V.22) and 2400 bps dx (V.22bis) ...

For products: 6NH7810-0AA30
12/17/2007
ID: 19354401
(0)
FAQ Which settings are required in order to operate an MD3 dial-up modem as a dedicated-line modem in the SINAUT network?

  Configuration notes: As a general rule, the MD3 must be at least release 4 in order to operate the dial-up modem as a dedicated-line modem. ...

For products: 6NH7810-0AA30, 6NH7810-0AA20
10/18/2006
ID: 24045211
(0)
Application example Modem Connection between S7-300 Stations via serial CPs

Task:   A frequent task is to transfer small to medium size data volumes from one S7-300 station to another S7-300 station as simply and cost-effectively as possible. Communication of both controllers should run via a telephone system so that the distance between both stations plays a s...

09/12/2006
ID: 21364749
(1)
 
Entries per page: 20 50 100
...
1
2
...