×
Siemens Industry Online Support
Siemens AG
Критерии фильтрации сообщений
Все продукты Моя продукция
Дерево продукции
 
 
Снять все фильтры
Продукция
Искать продукцию
Тип сообщения
 
Дата
Задача
  • Сохранить фильтр
  • Загрузить фильтры
  • Эл. сообщение в случае обновления
20
Сообщения
с фильтрацией по
'
scalance diagnostics data
'
и
'
Часто задаваемые вопросы
'
 
Сообщений на страницу: 20 50 100
...
1
...
Часто задаваемые вопросы How do you transmit the diagnostics data of an OSM, ESM or SCALANCE to the TFTP server using the Trivial File Transfer Protocol (TFTP)?

Sending the diagnostics data to the TFTP server ... order to send the diagnostics data to the TFTP server, ... the web-based management of SCALANCE X-200, SCALANCE X-300 and SCALANCE X-400 you select the ... Save & Load TFTP".... The diagnostics data of the OSM, ESM and SCALANCE network components can be ... Trivial File Transfer Protocol.... Sending the diagnostics data to the TFTP server... In the web-based management ... button to send the diagnostics data to the TFTP server.... Settings in the ... OSM, ESM and SCALANCE... Settings in the ... OSM, ESM and SCALANCE Make the settings ... the network components.... Note With SCALANCE you can also ... save event logs.

20.09.2010
ID: 44901238
(0)
Часто задаваемые вопросы Which ports are used by the various services for data transfer via TCP and UDP and what should you watch out for when using routers and firewalls?

Using HTTP you access the web ... CP to monitor device and process data and to use the web diagnostics functions.... With SCALANCE products, remote configuration is possible with ... CLI (Command Line Interface) via Telnet.... You enable or disable the ... (Command Line Interface) of the SCALANCE products.... TFTP is used with SCALANCE products to download firmware or save and load configurations.... SCALANCE X with Management functions... SCALANCE ... 7) SCALANCE W in compliance with IEEE ... supports Network Time Protocol (NTP).... 8) SCALANCE X-300, X-400 and X-500 can be used as Syslog clients.

05.07.2017
ID: 8970169
(17)
Часто задаваемые вопросы How do you record the data flow with TAP 104 and import it into SINETPLAN?

To determine the data flow between the ... distributed IO, the SCALANCE TAP104 has to ... the distributed IO.... The SCALANCE TAP104 is for ... of the bidirectional data traffic between CPU and distributed IO.... Here, the SCALANCE TAP104 is completely ... not affect the data traffic.... Using the SCALANCE TAP104 you can ... PROFINET and NRT data flows transparently and ... of the plant.... In addition, in ... to which the SCALANCE TAP104 was connected.... The data connections to be ... ports with brackets.... When the capturing starts, all the data flows are captured.... In the "PCAP ... source and target data are entered automatically.

17.05.2018
ID: 109756484
(0)
Часто задаваемые вопросы How can you use the SINEMA server to make simple changes to the configuration of SCALANCE devices?

109749379, V1.0, 08/2017 23 S ie m e n s A G 2 0 1 7 7 A ll ri g h ts ... SINEMA Server 3.1 Checking the Execution Results of a Script Wait for/monitor execution A sample script has been executed on two non-compatible SCALANCE X-200 devices to demonstrate troubleshooting.... This user data is used for logging on to the desired network device.... In the "User data for device access" area you enter the user data... Note If the network devices to be configured have different user data, a separate job has to be created and executed for each user data pair.

16.08.2017
ID: 109749379
(2)
Часто задаваемые вопросы Which PROFINET nodes support the extended PROFINET diagnostics and what do you have to configure?

 s Which PROFINET IO devices support the extended PROFINET diagnostics... 23678970 Module Article number Firmware ET 200ecoPN ET 200ecoPN 6ES7 141 ... components PN/PN coupler 6ES7 158 3AD00 0XA0 1583AD00 1583AD000XA0 from V1.0 SCALANCE X200x IRT products - from V2.1 SCALANCE X200 products - from V2.1 SCALANCE X300 products - from V2.1 SCALANCE X414-3E1) - from V2.1.1 SCALANCE X408-2 - from V2.0 SCALANCE X408-4C - from V5.0 SCALANCE X408-8C - from V4.1 SCALANCE X416-4C - from V4.1 SCALANCE X500 products - from V3.0 Gateways IE/AS Interface Link PN/IO Single AS-i Master:

20.01.2016
ID: 23678970
(5)
Часто задаваемые вопросы How do you use SINEMA Server for a firmware update von SCALANCE devices?

To be able to download the firmware to the SCALANCE devices you have to install a TFTP server or access an existing TFTP server.... Parameterize the TFTP server Start the TFTP server and assign it the proper IP address, in other words make sure that the TFTP server IP can be reached by all the SCALANCE devices to be upgraded....  2.2.4 Store TFTP Data SINEMA Server does not have its own TFTP server.

21.09.2016
ID: 109740213
(0)
Часто задаваемые вопросы How do you load the 3D, CAx and ePLAN data for the SIMATIC products?

Instructions In the global support database of Siemens you will quickly and easily find the latest information about the 3D, CAx and ePLAN data... Depending on the availability of the products, you can load the following data... Connection diagrams and data sheets... We recommend proceeding as follows to download the CAx data of the SIMATIC products.... Then click "Continue" to open the dialog for selecting the CAx data types.... Now you can download your data

24.06.2014
ID: 89671877
(2)
Часто задаваемые вопросы How is a VPN tunnel between two SCALANCE S S61x modules configured in Routing mode via the internet?

Diagnostics Both modules, the SCALANCE S61x A and B, ... in the control center.... Under "All Modules" you ... to transfer the configuration data to the SCALANCE S61x A.... Under "All Modules" you ... to transfer the configuration data to the SCALANCE S61x B.... In STEP 7 you ... or read out the diagnostics buffer of the CPU / Industrial Ethernet CP.... The SCALANCE S61x modules are operated in Routing mode.... The SCALANCE S61x V2 modules must ... mode from firmware V2.1.... The current firmware V3.1.0.1 for the SCALANCE S612 V3 is ... Entry ID 68041706 ... You need the ... higher to configure SCALANCE S61x V2 modules.

27.06.2013
ID: 24968210
(1)
Часто задаваемые вопросы How do you configure a VPN tunnel between a PC station and SCALANCE S61x via the Internet with the 2008 edition of SOFTNET Security Client?

32447942 15 4 Establish ... between PC station and SCALANCE S61x via the Internet.... Starting the SOFTNET Security ... Client with Start SIMATIC SCALANCE Security SOFTNET Security Client.... When you haven't ... configuration of the SCALANCE S61x and SOFTNET ... Client is saved.... If the VPN ... successfully and the SCALANCE S61x is reachable ... the column "Status".... Figure 4-1 loading the configuration data Open und load ... configuration file "Configuration2.SOFTNET.dat".... cer" file of ... as the configuration data... 32447942 16 In ... saving the configuration data in the configuration file.

23.08.2010
ID: 32447942
(0)
Часто задаваемые вопросы How do you configure a VPN tunnel between a PC station and SCALANCE S61x V2.1 via the Internet with the SOFTNET Security Client Edition 2005 HF1?

Now compile and save the configuration data for the SOFTNET Security Client (SSC) and the SCALANCE S 61x V2.1 ... set out below.... In order to transfer the configuration data to the SCALANCE S 61x V2.1, mark the SCALANCE S 61x V2-type ... the "Load" button.... On standard router ... on the connected Scalance S 61x.... In order to ... you require the SCALANCE S 61x with ... Configuration Tool V2.1.... A fixed external ... on the passive SCALANCE S 61x (B).... Passive means here that the SCALANCE S 61x (B) ... the tunnel setup.... The CPU 315-2 ... protected by the SCALANCE S 61x V2.1.... The SCALANCE S 61x V2.1 ... CPU 315-2 PN/DP.

26.10.2009
ID: 24953806
(0)
Часто задаваемые вопросы How do you read out the status of an MRP ring in the user program of the CPU in STEP 7 V5.x?

To determine the diagnostics address of SCALANCE X208 (redundancy manager), you mark SCALANCE X208 in ... Configuration.... The diagnostics address of the ... interface of the SCALANCE X208 is at ... X1 in "Diagnostics ... column.... To enable the diagnostics alarm in SCALANCE X208 (redundancy manager) ... PROFINET interface of SCALANCE X208.... Use the diagnostics ... Note Specify the diagnostics address of ... In this example you specify the diagnostics address 2041 (dec) ... For this you enable the diagnostics interrupt in ... In the "Media ... enable the "Diagnostics ... Diagnostics OB OB82 If ... CPU using the diagnostics ... In this example a SCALANCE X208 is used

27.04.2017
ID: 109483256
(13)
Часто задаваемые вопросы How do you configure a common MRP ring and the topology with two projects?

If a module displays an error, use the TIA Portal diagnostics to search for the cause and clear the error.... 109741671, V1.0, 10/2016 8 S ie m e n s A G 2 0 1 6 A ll ri g h ts r e s e rv e d Create device proxy data 1.... In the project navigation you open the menu of your configured controller and switch to the item "Device proxy data".... Double-click "Add new device proxy data".... Select the desired content for the export and export it via the "Export device proxy data" button.

26.10.2016
ID: 109741671
(2)
Часто задаваемые вопросы How do you transfer network information from the SINEMA Server to SCADA systems?

Table 2-2 No. Component ... 1556AU000BN0 172.16.9.32 255.255.0.0 7 SCALANCE XM408-8C 6GK5 408 8GS00 ... 172.16.9.40 255.255.0.0 8 SCALANCE XF208 6GK5 208 ... 172.16.9.41 255.255.0.0 9 SCALANCE XF208 6GK5 208 ... 172.16.9.42 255.255.0.0 10 SCALANCE W774-1 RJ45 6GK5 ... 172.16.9.80 255.255.0.0 11 SCALANCE W761-1 RJ45 6GK5 ... 172.16.9.81 255.255.0.0 Display data In the following ... instructions the following data is to be ... higher-level HMI system.... Network information like ... information from a SCALANCE XF208: ... 109740549, V1.0, 10/2016 ... Note that the data types "Array [] ... Server V13 SP1.

12.10.2016
ID: 109740549
(0)
Часто задаваемые вопросы Is cross-subnet PROFINET IO communication possible?

TCP/IP TCP/IP protocols are for parameterizing and configuring as well as for transferring diagnostics data... Real-Time RT Real-Time (RT) protocols are for cyclic high-performance transmission of user data... Isochronous Real-Time (IRT) Isochronous Real-Time (IRT) protocols are for synchronous transmission of user data

22.03.2016
ID: 109479139
(1)
Часто задаваемые вопросы SNMP application cases

The SNMP/OPC server of ... integration of the network diagnostics data and the process data available.... To enable diagnostics of SPS-based and PC-based ... as a standardized protocol.... SNMP has been used ... a standardized protocol for diagnostics of TCP/IP networks.... HMI systems today have ... standardized access to SNMP data... Both sets of data can thus be configured centrally.... From the system operator's ... SNMP is that data from the network ... is also visible.... With terminal devices, ... direct communication of data with the Ethernet interface modules.... All data services of the ... system with process data

30.04.2003
ID: 15166742
(0)
Часто задаваемые вопросы SIMATIC Remote Services - 'Preventive' module: How do you collect device and diagnostics information with the SAS DC?

This data includes, for example, information about the SCALANCE network components and diagnostics files.... Select Task" you select the task "Collect diagnostic and service data from SCALANCE devices only".... This data includes, for example, information about the S7 CPUs used in the project and the corresponding diagnostics buffers.... This data includes, for example, information about the computer and diagnostics files of the SIMATIC software.... Procedure The Data Collector of the SIMATIC Assessment Suite (SAS DC) collects diagnostics and system data via the network.

25.10.2016
ID: 109485717
(4)
Часто задаваемые вопросы Diagnostics of PROFINET devices

PROFINET IO has a manufacturer-neutral structure for data records with diagnostics data... Diagnostics data is created for defective channels and not for complete stations.... What diagnostics options do I have for PROFINET devices?... The diagnostics paths available with STEP 7 ... also available for PROFINET IO.... In addition the active network components like SCALANCE X switches or Industrial WLAN components SCALANCE W can be configured and ... TIA engineering tool STEP 7.... The Industrial Ethernet switches SCALANCE X-200 and SCALANCE X-400 can also be integrated ... a network management system.

05.10.2004
ID: 19549945
(0)
Часто задаваемые вопросы What should you watch out for with configured topology and the use of non-CiR-compatible IO devices?

During the failure there is no switch diagnostics data available in the H system.... It is planned that SCALANCE switches (XC-200, XF204-2BA and XP-200) recommended for the process industry will in future support CiR via a firmware update.... It is planned that SCALANCE switches (XC-200, XF204-2BA and XP-200) recommended for the process industry will in future support S2 and CiR via a firmware update.

Для продукции: 6ES7658-...58-....
30.08.2017
ID: 109749355
(0)
Часто задаваемые вопросы ATEX approval for use in hazardous zones for 3SB3 pushbuttons and indicator lights

PROFIBUS has integral diagnostics functions and can also be used for HART devices.... SIMATIC S7 controllers- SIMATIC ET 200 distributed I/Os- SIMATIC HMI Panels, Panel PCs and Thin Clients- SIMATIC NET, SCALANCE communications products•... In this purely electrical network, small volumes of data and energy are transmitted across the same bus cable.

15.11.2016
ID: 36999911
(0)
Часто задаваемые вопросы In the user program of an S7-300 or S7-400 CPU with integrated PN interface, how can you read out the current topology of the PROFINET IO system connected?

Thus, at the ... you specify the diagnostics address 0x7F5 of Port 5 of SCALANCE X208.... end data record transfer ID DWORD Diagnostic address INDEX INT Data record number ... INT Max.... At input parameter ... you specify the diagnostics address of the ... be read.... The distributed component is the SCALANCE X208 that is ... IO device.... In this case, ... 5 of the SCALANCE X208....  3.2 Parameterizing ... you read the data record with the ... ID.... In this example, you read data record number 802A ... component.... perform data ... REQ=0:... Table 3-2 Parameters ... VALID BOOL New data record has been ... BUSY=1:... 5 = true ... perform reading of data record ... (hex).

05.10.2009
ID: 38566021
(1)
 
Сообщений на страницу: 20 50 100
...
1
...
Поддержка статистики
Данная функция позволяет выдавать идентификаторы (ID) результата поиска согласно желаемому количеству (формат .txt)

Генерировать список
Копировать URL
Панель управления mySupport
Ссылки по теме