×
Siemens Industry Online Support
Siemens AG
  • 内容
  • 搜索
  • Service Cooperation
  • Digital Industry Services
    • Industrial Security Services
    • Industrial Network Validation
    • Energy Analytics
    • Digital Drive Train Services
      • Remote Support
      • Gear Unit Condition Monitoring
      • Mobile Diagnostics
      • Remote Diagnostics
      • SIDRIVE IQ Services
      • Energy Performance Contracting
    • Productivity Improvement
    • SINUMERIK Virtual Commissioning Services
    • SINUMERIK ONE Virtual Commissioning Services
    • SINUMERIK Service Assistance
    • NX Virtual Machine Tool Services
    • Remote Data Acquisition Services
    • OEE Analytics
    • Smart Service Scheduler
    • Remote Learning
    • Predictive Services for Presses
    • Predictive Services for Drive Systems

    Energy Performance Contracting



    Lifting competitiveness by increasing productivity is the most common and recurring challenge in industry. The options for investment outside of your core-business such as energy efficiency improvements are a possible lever, but savings uncertainty is a common showstopper for these projects. In addition, when given a narrow investment choice between a production-related project versus energy efficiency, the decision is always clear.

    What if there was a way to make an energy efficiency project more certain than a core-business opportunity? And rather than having to make a choice, what if you could invest in both opportunities? Energy Performance Contracting for drive applications from Siemens does just that.

    Energy Performance Contracting for drive applications pays for optimization measures through savings in energy costs. The projects are implemented according to a four-step process with low risk for our customers thanks to the promised savings.


     

    Your benefits at a glance with Energy performance contracting

    Drive applications, which account for nearly two thirds of industrial electricity use, represent one of the biggest opportunities for electricity and cost savings. Savings of up to 30 percent can be achieved within drive applications. The projects are structured so that only a portion of the savings are used for the service rate and the rest of the savings remains as a direct benefit for the customer. This makes the decision in favor of such a project easy: Energy Performance Contracting entails low risk in the project development phase and offers strong savings certainty. All this makes Siemens the perfect partner for your next energy efficiency project!


    Proceed as follows

    YourSiemens Contact Person is happy to answer questions on the Digital Industry Services or directly send an e-mail to: enpc.industry@siemens.com.


    Further Information

    109474259
    对统计的支持
    用该功能可根据所需数量输出搜索结果的IDs (格式 .txt)

    生成列表
    复制URL
    在新设计中显示此页面
    mySupport Cockpit