8/22/2017 7:00 PM | |
Joined: 8/31/2005 Last visit: 5/21/2024 Posts: 2197 Rating: (326) |
It's not TIA portal in general, but S7-1200 and S7-1500: https://support.industry.siemens.com/cs/ww/en/view/90885040 chapter 4.2 |
Last edited by: miami at: 8/22/2017 7:03:26 PM |
|
This contribution was helpful to2 thankful Users |
8/23/2017 3:39 PM | |
Joined: 7/7/2010 Last visit: 6/7/2024 Posts: 14771 Rating: (2378)
|
If you create a function block (FB/FC) and want it to work anywhere without change, you should avoid M-type memory *INSIDE* the block. Instead, you should pass in parameters that would be M-bits/M-bytes/M-words as parameters, and give them a good name. Then inside the block, #GoodParameterNames works quite nicely for any logic, calculation, and so on you might need to do. THAT is what they are trying to convey in that section of the documentation.
|
science guy |
|
This contribution was helpful to2 thankful Users |
Follow us on