12/22/2024 3:29 PM | |
Joined: 9/27/2006 Last visit: 9/18/2025 Posts: 12413 Rating:
|
Hello Elyas; Duris is right that the CPU you mention is from VIPA (now Yaskawa). You can confirm this from this manual: https://www.int-technics.pl/media/2011/07/hb97e_cpu_06-29.pdf VIPA CPUs are often very close to S7-300 PLCs, since they are basically a clone of the old Siemens S7-300s, but some operational differences exist. Butt i have used Profibus masters from other manufaxturers (Rockwell, GE Fanuc, Modicon...) with a DP/P coupler, with good sucess. Duris stated, please review the configuration of both masters to a ouple, s shown in the following manual, tis very well could be the source of your problems. https://support.industry.siemens.com/cs/ca/en/view/1179382 Notice that the Inputs of master 1 become the outputs of master 2, and the outputs of master 1 bcome outputs in master 2: Hope this helps, Daniel Chartier |
This contribution was helpful to
1 thankful Users |
Follow us on