(0)| 2/18/2025 10:51 PM | |
|
Joined: 5/30/2013 Last visit: 12/22/2025 Posts: 5 Rating:
|
Hi, i have a MMC 6ES7953-8LJ30-0AA0, 512KB. from a S7-300 plc that had an electrical problem and its communication ports were damaged. I inserted the memory into another good plc, but can't put it online and download the program inside it. I did a image of MMC with S7imgRD and WinHex programs, in both the image had 29.9MB. Do you think that if I write the image that I have in the same MMC, with S7imgWR the problem will be fixed? attach screenshot of the image obtained in winhex Jarod_Mk ------------------------------------------------------------------------------------------ |
Last edited by: Moderator_Lan at: 02/19/2025 09:12:42New subject after splitting |
|
Follow us on