12/21/2021 7:23 AM | |
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating: (877)
|
Hello syd_b, In order to confirm your feasibility of downgrade of firmaware, please check below points. 1. Please check the complete artcile number of drive with options installed. e.g. 6SE7021-8TB51-1AA1-Z xx xx 2. Check & note the existing firmware version of both drives. You can find istalled firmware details in & as - The first and second position of the firmware version can be read out in r069.01 and the third position corresponds to the first position after the decimal point in r828.01=0.1 (e.g. V1.32 corresponds to r69.01=1.3 and r828.01=0.2). From the above information, please visit this or this page & you can down compatible firmware version file & downgrade the firmware. Hope this helps.
|
Follow us on