4/5/2009 9:26 AM | |
Posts: 16 Rating: (0) |
Dear All, I m trying to get online S120 CU320 V2.5.sp1with CP5512 profibus adaptor I m getting error (Attached screen shot). If I m using MPI adapter then showing the accesible node and getting uplod, butafter cliking connect to the target system it is not connecting. Kindly give me the solution. AttachmentCP5512 error.pdf (444 Downloads) |
4/5/2009 10:53 PM | |
Joined: 5/17/2006 Last visit: 2/26/2024 Posts: 218 Rating: (26) |
Hello , Have you tried to change-> control panel -> set pg/pc interface Then select the card as profibus... as here and one link about 5511 , same settings cp card Best regards, |
Genetic Fuzzy PID Controller |
|
Follow us on