2/28/2023 2:52 PM | |
Joined: 2/28/2023 Last visit: 11/12/2023 Posts: 1 Rating:
|
Dear All, I'm very happy to find this very useful information available on this forum. It would be great if I can get some expert help via here. I'm trying to get a 1FT5046 motor running with a 6SN1123-1AA00-0HA1 ( LT modul int 8A) and the older 6SN1118-0AA11-0AA0 (not 6SN1118-0AA11-0AA1). I also have a 6SN1146-1AB00-0BA0 611 POWER SUPPLY MODULE. I also have the required motor cable (to bottom A1 connector) & motor encoder cable (to front X311 connector) to connect the motor to the 6SN1123 + 6SN1118 drive So I think I have all the basic components but I only have very little to no clue how to get everything properly connected and setup to get it basically running / PID tuning via +/- 10V analog control. Especially how to setup / connect all the various terminals on the front of the 6SN1146 and 6sn1118 modules is unclear to me. Any help would be highly appreciated. Best regards, Francois ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 03/01/2023 09:42:27New subject after splitting Last edited by: loonvf1 at: 03/08/2023 14:41:26 |
|
3/12/2023 4:57 AM | |
Joined: 10/17/2007 Last visit: 9/4/2024 Posts: 4012 Rating:
|
I attached manual for your 611A system Don't worry about 6SN1118-0AA11-0AA0 or 6SN1118-0AA11-0AA1 they are same function For power supply read manual Chapter "Supply Infeed ( NE) " For the drive module Read Chapter Feed Module (VS) I give you some short tips: #1--6SN1146-1AB00-0BA0 611 POWER SUPPLY MODULE. you need read manual connect 3 AC input power, then connect flat cable (lower voltage /control power) and P600 and M600 (DC600V bars) to the drive module. For enable--connect switch or wires jumper Terminal 63 to 9, 64 to 9, ter.112 and 48 to 9. also jumper NS1 to NS2 , when you see Yellow LED on and Green LED off, means Power module enabled you can measure DC 600V (+/- 20V) on P600 and M600 #2--6SN1118-0AA11-0AA0 should insert into 8A drive box, for enabling , connect Ter.65 to 9 and 663 to 9. speed reference --connect battery box (max 10VDC) to Ter.56 /14 you need to read Page VS/1-5 the form to use for match you motor to the drive. Taking out Parameter Sub-module from 6SN1118-0AA11-0AA0, set dip switch on/off following the form Please feedback and if you think my answer helps please rating
Attachment611A_1000_en.pdf (671 Downloads) |
Last edited by: nulizhang at: 03/12/2023 05:03:15If you have used module you also need check NS1/NS2 If you like my comments please |
|
Follow us on