6/4/2009 9:47 PM | |
Posts: 5 Rating: (0) |
Hi everybody I´m tryingto move a Conveyor Beltin three differents RPMs, 400rpm,600rpm and 800rpm.Could I use a LOGO!with a Drive Converter? Thanks For All. |
6/4/2009 10:09 PM | |
Joined: 1/5/2007 Last visit: 4/7/2023 Posts: 1690 Rating: (580)
|
Hi Waldo, yes it is possible. i think you need a 0..10 V analog output from the LOGO!. Then you must use an addidional Module AM2 AQ. The circuit can be only an analoge multiplexer and a textbox to put in the 3 (max. 4) different values. To define the values you need the correlation of rpm to voltage. To give you more help we need more infos about your application. Best regards Betel Hi LOGO!Barbarian, that are some interrest circuits, thanks. Best regards Betel _________________________________________________ Perhaps helpful links: Collection of notes and circuits for the use and programming the LOGO! Scalingof signals with analog blocks retreving data from logo |
==> Meine TAG-Listen: "deut." |
|
6/4/2009 10:58 PM | |
Joined: 1/5/2007 Last visit: 4/7/2023 Posts: 1690 Rating: (580)
|
Hi Waldo, how do you want to connect the motor to the logo and witch type are the needed output signals: digital (relais), analog 0..10V or 0(4)..20mA ? Have you a data sheed of the motor? Best regards Betel _________________________________________________ Perhaps helpful links: Collection of notes and circuits for the use and programming the LOGO! Scalingof signals with analog blocks retreving data from logo |
Last edited by: Betel at: 6/4/2009 11:20 PMcorrect links ==> Meine TAG-Listen: "deut." |
|
6/5/2009 12:04 AM | |
Posts: 5 Rating: (0) |
the Logo has digital outputs(relais), Some data of the motor are: Motor Three-Phases,1.7HP, 50 Hz, Delta Connection 220VAC, 5.25A, 1425rpm. |
6/5/2009 8:41 AM | |
Posts: 153 Rating: (16) |
Hi, all. Micro Automation Set 12:
The application on Logo! and the instruction in the attachment. Attachmentfile_microset12.zip (728 Downloads) |
Last edited by: Andrey [Str] at: 6/5/2009 8:56 AM |
|
Follow us on