1/14/2021 2:20 PM | |
Joined: 2/29/2016 Last visit: 10/17/2023 Posts: 1 Rating: (0) |
Hi, Have you found the solution? Because I am having the same issue with a servomotor 1FK7022-5AK21-1VA3. I am trying to do the commissioning with a S120 drive through Starter... It would be nice if anyone can help. ERROR 7990: drive incorrect motor data identification (103) 103: Maximum frequency exceeded during the rotating inductance measurement. ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 01/15/2021 08:34:12New subject after splitting |
|
1/15/2021 4:29 PM | |
Joined: 7/7/2010 Last visit: 9/12/2024 Posts: 15180 Rating: (2417) |
That Siemens motor, is it a Drive-cliq™ motor? I don't think so. However, if it is a drive-cliq motor and it is not able to perform a motor ID, perhaps you should not do one and see if it performs properly without tuning. If it is not a Drive-Cliq motor, what parameters have been entered during the Starter motor setup wizard? Did you use the nameplate, or the datasheet for that part #? Is it possible this motor has the wrong nameplate? The datasheet provides some specifics which can be measured. What version of Starter are you using, and what firmware in your CU310-2/320-2? Starter commissioning wizard, was your motor available from the list of motors, or did you have to manually enter motor configuration parameters, or both?
|
science guy |
|
3/22/2022 6:08 AM | |
Joined: 9/18/2015 Last visit: 9/9/2024 Posts: 45 Rating: (1) |
I get the same fault. They are siemens drivecliq motor. Can anyone help? 6SL3120-2TE15-0AD0 with Siemens Synchronous motor 1FK7062-2AF71-1QG0 |
3/22/2022 8:01 AM | |
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating: (877) |
Hello, 6SL3120-2TE15-0AD0 is double motor module 5A/5A capacity. 1FK7062-2AF7.-.... is 1.9 KW motor 8.5 Nm. Please check if the motor is connected to correct port i.e. X1 or X2 of double motor module. |
This contribution was helpful to1 thankful Users |
Follow us on