12/8/2023 9:00 PM | |
Joined: 2/10/2021 Last visit: 6/12/2024 Posts: 2 Rating:
|
Can anyone explain the behavior in the image attached here? Specifically, - the counter B008 can only increment if the value of Q2 is 0 and the value of Q3 is 1 - Q3 feeds the Q2 Relay Coil, so the Q3 Relay Coil should be evaluated before the Q2 Relay Logic - If the value of Q3 is 1, then, because that Q3=1 feeds an OR instruction before the Q2 Relay Coil, the logic feeding the Q2 Relay coil should never write a value of 0 to Q2 when Q3 is 1. The environment is LOGO!Soft Comfort Demo version 8.3.0 (2021-03-08 13-30) running the Simulator. More detail on the application is available at this link. ------------------------------------------------------------------------------------------ |
Last edited by: drbitboy at: 12/08/2023 21:06:03Last edited by: drbitboy at: 12/08/2023 21:42:18Last edited by: The Helping Hand at: 12/11/2023 09:53:18New subject after splitting |
|
12/9/2023 3:25 AM | |
Joined: 12/18/2014 Last visit: 7/16/2024 Posts: 33361 Rating:
|
Please don't post twice for the same problem. You also make a own topic for your problem. LOGO! unexpected behavior
|
This contribution was helpful to
1 thankful Users |
12/11/2023 9:54 AM | |
Joined: 8/21/2014 Last visit: 7/16/2024 Posts: 999 Rating:
|
Closed cause question posted twice. The second thread with the subject LOGO! unexpected behavior is published within the conference LOGO! - Software Best regards, |
My Forum is the place to personalize your profile, |
|
Follow us on