5/17/2024 6:57 AM | |
Joined: 4/24/2006 Last visit: 7/3/2024 Posts: 8707 Rating:
|
Hello, Perhaps this link might help: Best regards, Wizard |
5/24/2024 12:24 PM | |
Joined: 8/3/2009 Last visit: 7/3/2024 Posts: 13187 Rating:
|
Hello FRANCK HERVE I´m afraid that you cannot connect the HMI Simulation of a Basic Panel 1st Generation to a PLC Sim V15 PLC. Check this FAQ: https://support.industry.siemens.com/cs/de/en/view/109742764 Since V14 they have changes something in PLC SIm and so older HMI Images than V14 cannot connect to it any more in simulation. And the Basic Panels 1st Gen have only a V12 image available Which real HW it should run. Bye Murof |
If this Information really helps, you could use the Rate function |
|
Follow us on