5/17/2024 10:34 AM | |
Joined: 8/24/2023 Last visit: 6/13/2024 Posts: 1 Rating: (0) |
Query: Unable to Access Variables in WinCC RT Advanced SCADA from Sinumerik 828D via OPC UA I am using WinCC RT Advanced SCADA to communicate with a Sinumerik 828D CNC controller. The communication is set up using OPC UA, with the Sinumerik 828D configured as the OPC UA server and WinCC RT Advanced as the client. After successfully connecting the OPC UA client in WinCC RT Advanced to the OPC UA server on the Sinumerik 828D, I can see the server but I am unable to access or read the necessary variables/parameters. I have verified the connection using the UaExpert software, and it shows successful communication and visibility of the variables. However, when attempting to fetch the Sinumerik data in WinCC RT Advanced, I cannot access the required variables. I am currently on-site and need urgent assistance to resolve this issue. Could you provide guidance on how to access these variables in WinCC RT Advanced? ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 05/17/2024 11:41:30New subject after splitting |
|
Follow us on