5/23/2024 8:20 AM | |
Joined: 3/9/2023 Last visit: 6/7/2024 Posts: 27 Rating: (1) |
Hi dear all, I use TIA v17 and I run the PLC program in PLCSim Advanced 5.0. Now that I want to connect physical KP300 to this system. I have assigned IP adress and profinet name and downloaded the hmi program thru network .I also can ping the KP300. (please see attached screenshots) However, I can not see hmi tag values on the KP300. It shows #####. Any ideas on problem? ------------------------------------------------------------------------------------------ Attachmentkp300_basic_mono w PLCsim Advanced.pdf (24 Downloads) |
Last edited by: The Helping Hand at: 05/23/2024 13:11:14New subject after splitting good day to be alive, sir, |
|
Follow us on