6/17/2024 5:19 AM | |
Joined: 2/25/2016 Last visit: 9/27/2024 Posts: 12 Rating: (4) |
Good afternoon, has anyone tried making a CustomWebControl to display 3D files with ThreeJS library. I am doing experiments and have had some success on WinCC Runtime (Windows). But here is a question whether the same component will work on HMI panel? Such as MTP700 for example. Can anyone test these two components, one checks if WebGL technology is supported on the panel and the second one should actually display 3D object (Hourse). AttachmentCustomWebControl.zip (140 Downloads) |
6/25/2024 10:28 AM | |
Joined: 2/25/2016 Last visit: 9/27/2024 Posts: 12 Rating: (4) |
Wow great news, so it said WebGL was supported? I changed the component with the Horse, I think it should load faster now, but wonder if it will work on the panel? It now work on WebGL Render not Canvas Render. It would be great if you have the ability to test on your MTP1000 panel. Attachment{024D7BB2-A9AA-4E66-A280-E09C88F88322}.zip (94 Downloads) |
6/26/2024 9:13 AM | |
Joined: 1/20/2018 Last visit: 9/26/2024 Posts: 36 Rating: (4) |
manifest.json file has a comma missing and zip file is incorrect. ftfy.
Attachment{024D7BB2-A9AA-4E66-A280-E09C88F88322}.zip (95 Downloads) |
Last edited by: ender1adam at: 06/26/2024 09:19:48Last edited by: ender1adam at: 06/26/2024 09:20:16 |
|
6/26/2024 12:06 PM | |
Joined: 2/25/2016 Last visit: 9/27/2024 Posts: 12 Rating: (4) |
Thank you! You are right, it was mistake in manifest.json I've fixed it. New file attached. Attachment{024D7BB2-A9AA-4E66-A280-E09C88F88322}.zip (95 Downloads) |
This contribution was helpful to1 thankful Users |
Follow us on