6/27/2024 7:13 PM | |
Joined: 4/1/2022 Last visit: 6/28/2024 Posts: 2 Rating: (0) |
Hello, i have similar problem. The actual current is normal but actual torque reached limit r1358 and the motor cant be speeder.For example i sent 1000 rpm referance but motor turns 500 RPM because of r1358. Also p1300=20 speed control encoderless As far as i know P1522 is positive torque limit, the value %150. Whrn i get torque limit fault i look actual torque %60-70. But r1358 always change as motor running. i dont understand why this value changes... Because the limit is a constant value as %150. So what is difference between torque limit(p1522) and effective torque limit(r1358). How can i let the motor can be speeder until actual torque %150. ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 06/28/2024 08:08:22New subject after splitting |
|
Follow us on