12/12/2020 11:56 AM | |
Joined: 7/3/2018 Last visit: 7/26/2023 Posts: 8 Rating:
|
Hi everyone, I have a TP 1200 Comfort Panel and I'm trying to log data on a Synology NAS, as I need to remotely access the data, following the Siemens application example Integrating HMI Operator Panels in TCP/IP Networks and access to a NAS or to a shared Windows folder (Entry ID:92346478), but it doesn't work. When I try to simulate it from TIA Portal on my PC it works, but from the TP doesn't, and there is no system error. Everything is in place, correct user with all right on the NAS, username and password inserted on the TP, but no way. I heard that this Siemens application is supposed to work on WinCC Runtime installed on Windows 7 or 10, and not on a TP with a Windows CE. In fact when I try to open the file explorer of the Windows CE of the TP and point to the NAS, it doesn't work. Anyone has any idea? Thanks. |
Last edited by: Jen_Moderator at: 12/14/2020 09:38:45Optimized link. |
|
7/1/2024 8:07 AM | |
Joined: 11/17/2016 Last visit: 7/1/2024 Posts: 2 Rating:
|
Hi everyone, I facing the same issue. Have u solved ur problem ? if yes, how ? best regards.
|
Follow us on