6/12/2024 12:52 PM | |
Joined: 10/12/2012 Last visit: 9/27/2024 Posts: 12 Rating: (0) |
Hi everyone, I have configured 1510sp1-pn and s120 cu310 - 2pn sinamics servo drive. Everything look green but at the TO side there is a configuration error. 1 ) MC Fatal error 101: Configuration error. (Sensor[1] must be configured for DSC.) MC component: PositioningAxis_1, TO_DB= 2 When I select encoder "Encoder2" which is external encoder connected at X23 it gives this error. 2) Also plc diagnostic side there is an error. "Error on partner - IRT not possible at this port" These errors are related with each other? Attachments120_to9.zip (338 Downloads) |
6/12/2024 12:54 PM | |
Joined: 10/12/2012 Last visit: 9/27/2024 Posts: 12 Rating: (0) |
Also you can see error diagnostics of plc. |
7/9/2024 10:25 PM | |
Joined: 10/12/2012 Last visit: 9/27/2024 Posts: 12 Rating: (0) |
There is no answer or solution :( |
8/7/2024 3:02 PM | |
Joined: 7/20/2024 Last visit: 9/9/2024 Posts: 12 Rating: (0) |
selam aynı sorun bende de var sız cozebıldınız mı |
Follow us on