2/14/2023 6:25 AM | |
Joined: 6/26/2008 Last visit: 7/30/2024 Posts: 50 Rating:
|
Hi, I downloaded and installed the (openness) add-in for import and export to TIA v18. From https://support.industry.siemens.com/cs/document/109773999 The add-in was saved as: It was activated in the Add-ins tab in TIA Portal. When trying to export a screen (left click>Export / Import) the following error occurs: The type 'Siemens.Simatic.Hmi.DL.ModernUI.ILScreenData' is not available with openness for the Engineering version V18. Openness was installed with TIA_Portal_STEP7_Prof_Safety_WINCC_Adv_Unified_V18 and SIMATIC_WinCC_UnifiedRT_V180_SR1_Upd1 was installed. Any ideas what could be wrong? Thanks |
7/10/2024 4:45 PM | |
Joined: 4/28/2015 Last visit: 8/13/2024 Posts: 36 Rating:
|
Hi, This Add-in does not support WinCC Unified devices, as the required APIs are not available. In this example some possible Features has been implemeneted but a complete and Import is not possible. https://github.com/tia-portal-applications/TIA-Add-In-ShowScripts/tree/V19 Regards Matthias |
This contribution was helpful to
1 thankful Users |
Follow us on