7/16/2024 2:31 AM | |
Joined: 1/16/2012 Last visit: 7/19/2024 Posts: 108 Rating:
|
Dear Experts, AttachmentBlock Protection.zip (16 Downloads) |
Last edited by: Tech Ahmed at: 07/16/2024 02:42:01 |
|
7/16/2024 5:32 AM | |
Joined: 1/27/2009 Last visit: 8/15/2024 Posts: 171 Rating:
|
Hello Tech Ahmed, You need to right click on the desired block and select Properties. Select Protection under the tab General. Click the button named Protection under the Know-how protection. Type in old password and click on Remove and protection will be removed. If you do not know the password, then protection cannot be removed. Please also take a look at this thread siemens 122363 In the older version of the Step 7 (Simatic manager), know how protections was realized by adding the line KNOW_HOW_PROTECT at the very top of the block. If the source of such a block is lost, then there is no possibility to unlock it legally. |
The only thing necessary for the triumph of evil is for good men to do nothing |
|
This contribution was helpful to
1 thankful Users |
Follow us on