7/15/2024 4:44 AM | |
Joined: 8/7/2023 Last visit: 7/22/2024 Posts: 5 Rating: (0) |
I run by WinCC RT Application, but when I start, the SCADA deactive after few second automatically. I try use "ccarchivemanager.exe -resetall" and start SCADA again and it works well. But I had read on the forum, someone said that "ccarchivemanager.exe -resetall" will reset the configuration at default (1 week for all segment and 1 day for single segment). Dose any solution for this problem ? Thanks ------------------------------------------------------------------------------------------ |
Last edited by: Wit_Moderator at: 07/15/2024 13:21:10New subject after splitting |
|
7/15/2024 4:42 PM | |
Joined: 7/19/2022 Last visit: 7/22/2024 Posts: 377 Rating: (61) |
Hello hien_ho145, It would be necessary to know in which process, during WinCC startup, it stops and prevents WinCC from running. Normally it is usually in processes related to TagLogging or AlarmLogging. For these cases check: |
If this Information really helps, you could use the Rate function |
|
Follow us on