7/31/2024 8:11 AM | |
Joined: 5/6/2022 Last visit: 11/19/2024 Posts: 495 Rating: (99) |
Hi AutoGen_4955742, First of all, I would like to tell you that since this is a discontinued display my knowledge is not very extensive but I would like to ask you the following: - I understand that you have correctly inserted the card in the panel, right? - Have you tried with other different cards to see if the same thing happens? - I would recommend resetting the panel to factory defaults and restarting it to see if the same message keeps popping up. Best regards!
|
If this Information really helps, you could use the Rate function |
|
7/31/2024 5:36 PM | |
Posts: 13 Rating: (0) |
The memory card was missing from the beginning. |
8/5/2024 9:09 AM | |
Posts: 13 Rating: (0) |
When I input the CF card, do I need to write the path to it? I am hope for your help |
Follow us on