10/3/2023 8:51 AM | |
Joined: 1/31/2018 Last visit: 10/31/2024 Posts: 20 Rating: (0) |
Hello In this summer i put this system which count the speed with a encoder (see the programm adove) and control the speed with a valve,the system has worked perfect.Now I a m trying to set up the same system but with a limit switch,i mean i have only one pulse to calculate the real meter per minute. For this purpuse i measuring the time interval between pulses,(can you see this in the attachemnt programm) ,the radious is 5cm,and after the count ,calculate the meter per minute ... I would like to see the programm and i want your comment if i am right with this way. ------------------------------------------------------------------------------------------ Attachmentmeter_per_minute_with_limitswitch_02082023.zip (463 Downloads) |
Last edited by: Jen_Moderator at: 10/13/2023 10:08:18New subject after splitting |
|
11/8/2023 8:03 AM | |
Joined: 1/31/2018 Last visit: 10/31/2024 Posts: 20 Rating: (0) |
Hello everyone Any suggestion or comment about this i had make with one limit switch?Its the right way ? |
8/23/2024 6:02 AM | |
Joined: 1/31/2018 Last visit: 10/31/2024 Posts: 20 Rating: (0) |
Hello Any objection about the meaure speed with one pulse?Also i have seperate the code for this purpose,i am waiting your comment about that Attachmentmeasure_mper_minute_withlimitswitch_23082024.zip (207 Downloads) |
Follow us on