6/27/2009 2:13 PM | |
Posts: 7 Rating: (0) |
Dear all, i want to know main diffrences between simodrive and masterdrive. |
6/27/2009 3:22 PM | |
Joined: 7/15/2008 Last visit: 10/6/2024 Posts: 382 Rating: (44) |
Hello ekansh I hope I can sum up the differnces without creating more confiusion. The Simodrive is a converter sytem that is mainly used in singel or multiple axis application like a CNC Machine controlled by a 840D, orin an application where you have multiple axis with difrrent motors working togehter to perform a task like a Robot or a Gantry The Masterdrive is a converter used for single motor application or where you havea masterdrive controlling multiple motors ( same model ). A good example is the use of a Masterdrive in an Elevator to lift pallets where you need good torque and speed. To get more and better info please visit theMotion Contol Website. https://www.automation.siemens.com/mc/mc-sol/en/8a7d5330-71a9-457b-852b-c615acef4ac6/index.aspx |
This contribution was helpful to2 thankful Users |
6/30/2009 9:03 PM | |
Joined: 12/20/2008 Last visit: 8/12/2024 Posts: 556 Rating: (236) |
I think this is more appropriate. |
Follow us on