4/9/2010 12:33 PM | |
Joined: 9/23/2005 Last visit: 10/9/2024 Posts: 4349 Rating: (1446)
|
Normally timers have used to act in variables. Sometimes however, the timers are just placed in the software without a connection of his outputs (e.g. to tests or measure time / represent it in a HMI). In this situation (using a Timer without a use of your outputs,) the timer will not run. To avoid this situation, use an auxiliary temporary variable (or any other variable attribution) to the Timer Outputs. See pictures in attachment AttachmentS7-1200 timer.pdf (1655 Downloads) |
Denilson Pegaia |
|
This contribution was helpful to4 thankful Users |
Follow us on