5/7/2007 12:13 PM | |
Joined: 10/31/2005 Last visit: 9/4/2024 Posts: 366 Rating: (31) |
Hello Iam, please check this:/tf/WW/en/Posts/9068 There you can find out which software you can use. |
Last edited by: Pandiani at: 07.05.2007 12:15Last edited by: Pandiani at: 07.05.2007 12:14Last edited by: Pandiani at: 07.05.2007 12:13 |
|
5/7/2007 4:51 PM | |
Joined: 10/11/2006 Last visit: 9/27/2024 Posts: 5908 Rating: (804)
|
Hello, following a extract from FAQ Id-Nr. 22642090 and the guide for changing to CUVC attached: The MASTERDRIVES Vector Control CU2 devices (end number of the MLFB 20 / 21) have been replaced by the MASTERDRIVES Vector Control CUVC series (end number of the MLFB 60 / 61). The version / type of control for all devices with a specified power section is always defined by the basic device module (e.g. CU2 or CUVC). If a new device is needed because a component in the power section of the existing device is defective, it is possible to fit the CU2 module from the old device into the new one. The new device then has the same functionality as the old one. A more advanced installation is not required. If a PROFIBUS communications module is fitted in the existing device, then please take note of entry ID 18310143 Attachmentguide_cu2_cuvc.pdf (466 Downloads) |
With best regards, |
|
Follow us on