2/14/2013 4:54 PM | |
Posts: 8 Rating: (0) |
Hi! Im trying to upgrade a Simatic HMI IPC477C by use of simatic image & partition creator v3.1 I have a panel with 4GB flash, and i have transferd the imagefile to a boot USB stick from kingston on 8gb. I reboot the panel and the partition software starts up. On the stick i have three files, that i found when i extracted the ziped image i got from siemens. 4x7_WinCC_V70SP3.PBF on 8kB 4x7_WinCC_V70SP3_0000p.000 on 2,2GB 4x7_WinCC_V70SP3_0000p on 30 kB When i start the simatic image & partition creator v3.1 i follow theese steps. - create with the Image&PartitionCreator CD a bootable USB-Stick with Image&PartitionCreator Best regards Calle L |
Last edited by: CalleLundin at: 2/14/2013 4:59 PMLast edited by: CalleLundin at: 2/14/2013 4:54 PM |
|
Follow us on