6/28/2013 7:01 AM | |
Joined: 5/17/2010 Last visit: 2/21/2022 Posts: 80 Rating:
|
Thanks Valli, But the one you provided is Server 2003 R2. I'm not sure that can be use, because the requirement is without R2.
|
6/28/2013 7:34 AM | |
Posts: 262 Rating:
|
Hi, I suggest to take this as a deviation point as in any case Windows 2003 is very old and can easily be upgraded to R2 with the help of microsoft people. refer the below link. http://support.microsoft.com/kb/912309. IPC will be loaded with WINDOW 2003 R2 only or WINDOWS Server 2008 etc... |
6/28/2013 8:38 AM | |
Joined: 5/17/2010 Last visit: 2/21/2022 Posts: 80 Rating:
|
Hi, What I need is a downgrade not upgrade, if the available version Windows Server 2003 R2. I have experienced with WinCC using Windows Server 2008 R1, and it's not compatible must downgrade to Windows Server 2008. I'm afraid that this will happen to PCS7 also, that's why I still search for Srver 2003.
|
7/1/2013 8:37 AM | |
Posts: 262 Rating:
|
Hi, |
7/31/2013 6:00 AM | |
Joined: 3/31/2009 Last visit: 7/16/2024 Posts: 191 Rating:
|
Hii, check this out : according to the compatibility, it should run with win2003 r2 ( with note ).. and it saya please refer to the readme on the cd of pcs7.. br rusli
|
Follow us on