1/8/2008 8:28 PM | |
Posts: 12 Rating: (2) |
Can the 3UF5 or 3UF7 inputs be connected using an external source of 110VAC. From what I see on the ordering information is the device uses its own onboard DC. |
1/9/2008 10:54 AM | |
Posts: 11 Rating: (0) |
Hi Dr Suess, external sources of 110 V can be used with digital expansion modules of Simocode. Kind regards |
Last edited by: 3UF at: 09.01.2008 10:55 |
|
1/9/2008 2:29 PM | |
Posts: 12 Rating: (2) |
Thankyou for the help. I forgot to look at the expansion modules. I only used the basic modules in the past. |
Follow us on