10/8/2008 9:43 AM | |
Posts: 661 Rating: (123) |
Hi, you could use a shift register. Please find the attached 0BA6 file. I connected also a switch to simulate the weekly pulses... In the first cycle the shift register gets activated (+B003) by using startup flag M8, then it gets deactivated again, when the first S-bit is ON. If the sequence is at the end (when S4 is ON) B003 gets set and it starts again. If you need more support, please attach your program. AttachmentShift register.zip (858 Downloads) |
Follow us on