9/2/2019 1:26 PM | |
Posts: 5 Rating: (0) |
Dear All, One of our customer had a mjor failure with his old MASTERDRIVE MC Unit Version: 025, whereby he replaced it with a Newer Version: MASTERDRIVE MC Plus Unit Version: 016. The system provides the following error when trying to download the parameters from the older unit into the newer version. Is it possible to downgrade the MASTERDRIVE MC Plus Unit Version: 016 into the previous MASTERDRIVE MC Unit Version: 025? What can be done in order to adopt the VFD into operation? I've enclosed the parameter download error picture. Thanks in advance. Tzvi ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 09/03/2019 09:24:48New subject after splitting |
|
9/3/2019 10:55 AM | |
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating: (877) |
Hello, Please note, original Master drive version is 2.5 (25). You are replacing it with version 1.6 (16) i.e. older & not newer. User can not load newer version parameters into older version. From your post, it is not clear whether customer is replacing only control card or drive unit. Please note, V 1.X can not run on new hardware. Please read Product announcement & Changeover Guidelines, MASTERDRIVES Motion Control to Performance2 this for more information. |
Last edited by: Jen_Moderator at: 09/03/2019 12:46:32Optimized links. |
|
Follow us on