10/28/2008 10:16 AM | |
Posts: 9 Rating: (0) |
Hello! I use LOGO!TD+0BA6. I have 8 inputs for errors(motor break,...).Does any one have idea how to display the errors on TD.(example in attach).I wanna use shift registers bit(if is possible) When the error is present user can see on display then when we don't have error in input, user have to press the button to eliminate the error. thx. Attachmenterror.zip (597 Downloads) |
10/29/2008 9:10 PM | |
Posts: 2930 Rating: (432)
|
Hi, check this example and have a look to the text messages (LSC V6.0) Acknowledgement should be enabled in each text message. I hope this helps Regards Helmut AttachmentError 1.zip (648 Downloads) |
Follow us on