6/24/2020 10:19 PM | |
Joined: 11/19/2019 Last visit: 8/21/2024 Posts: 10 Rating: (0) |
I'm having a similar problem. The cable winding system has a working torque control. The torque is calculated and applied according to the winding diameter, so small changes are normal, but a few days, the torque is insufficient or more. I set the p100 parameter from 4 to 3 to test the encoder but it gives f015 fault. What can be the reason for these problems? driver masterdrives vc ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 06/25/2020 09:26:55New subject after splitting |
|
Follow us on