12/9/2020 4:44 AM | |
Joined: 3/14/2020 Last visit: 4/27/2021 Posts: 8 Rating: (0) |
Hi all, I have simovert: 6SE7021-8TB61-Z , 6SE7024-7TD61-Z, 6SE7028-6EC85-0AA0, I have learned about this product line which has been disconnected and switched to the sinamic s120, now if i switched to a new one, I can choose which device is suitable for the old devices and should work with sinamic s120 current? Thanks everyone! Kind Regard, Tran Hoai Duc from Vietnam ------------------------------------------------------------------------------------------ |
Last edited by: The Helping Hand at: 12/09/2020 15:42:55New subject after splitting Last edited by: The Helping Hand at: 12/09/2020 15:44:15Spelling in topic subject |
|
12/9/2020 8:09 AM | |
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating: (877) |
Please do not create multiple posts. Read reply here. |
This contribution was helpful to1 thankful Users |
12/9/2020 3:45 PM | |
Joined: 8/21/2014 Last visit: 9/9/2024 Posts: 1018 Rating: (14) |
As already mentioned: closed, cause question posted twice. The second thread with the subject [Convert Simovert to Sinamic s120 ] is published within the conference [SIMOVERT MASTERDRIVES]. Best regards The Helping Hand
|
My Forum is the place to personalize your profile, |
|
Follow us on