6/3/2019 6:33 PM | |
Posts: 4 Rating:
|
I attach an example AttachmentSiemens support.zip (345 Downloads) |
6/3/2019 7:30 PM | |
Posts: 4 Rating:
|
Thank you very much for the information. I will prove and I will tell you the results.
|
6/4/2019 9:11 AM | |
Posts: 4 Rating:
|
It seems that the flash memory works, when there is power cut, and starts again. Another problem that I find is, when I put a value on the web, and I give a start from the entry V0.0, in the strategy add 256 to the value I have set. I attach screenshots and strategies. Thank you AttachmentSiemens support.zip (255 Downloads) |
6/4/2019 9:34 AM | |
Joined: 12/18/2014 Last visit: 7/31/2024 Posts: 33450 Rating:
|
There is only one VM memory, and this is byte-oriented in addressing. The range provided for the user goes from V0.0 to V850.7, ie 6808 bits or 851 bytes. VB (bytes in VM memory) = VB0 to VB850 Example: You are using Word 0 in VM memory = VW0 for your timer. The VW0 contains 2 bytes, VB0 and VB1. VB0 contains 8 bits, V0.0 to V0.7. VB1 contains 8 bits, V1.0 to V1.7. So if you're using VW0 for the timer, you can no longer use V0.0 to V1.7 for other things like starting the timer. AttachmentLOGO! 8 Soft Comfort Online-help 2016_07 (FS4) pages 111-126 (VM area).pdf (549 Downloads) |
This contribution was helpful to
1 thankful Users |
Follow us on