6/26/2024 11:27 AM | |
Joined: 12/18/2014 Last visit: 9/7/2024 Posts: 33710 Rating:
|
Do you already have a program approach? |
6/26/2024 11:57 AM | |
Joined: 12/18/2014 Last visit: 9/7/2024 Posts: 33710 Rating:
|
Here a suggestion for the points 1-3. For the points 4 and 5 I need more information to help. I don't understand your description to this points ,,,, AttachmentSetpoint adjustment via F-keys with limitation and start value_8.4.zip (141 Downloads) |
Last edited by: ixo65 at: 06/26/2024 11:59:03add attachment |
|
6/27/2024 8:57 AM | |
Joined: 12/18/2014 Last visit: 9/7/2024 Posts: 33710 Rating:
|
Here is the complete solution.
AttachmentSetpoint adjustment via F-keys with limitation and start value_8.4_V2.zip (142 Downloads) |
This contribution was helpful to
2 thankful Users |
7/4/2024 2:52 PM | |
Joined: 12/18/2014 Last visit: 9/7/2024 Posts: 33710 Rating:
|
See attachment.
AttachmentVariable_output_between_7V_and_10V_0BA8.Standard.zip (122 Downloads) |
This contribution was helpful to
1 thankful Users |
7/5/2024 11:21 AM | |
Joined: 5/13/2022 Last visit: 7/17/2024 Posts: 10 Rating:
|
Hi, something is not working correctly in the program. at setpoint 20 the output voltage is fine. at a different setpoint the voltage is not calculated correctly. been messing with it for a while but i cannot put my finger on it . do not have enough experience with the analog/ mathematics instructions. If you now what it is put in a small explanation if you have the time. try to learn from it all. thanks AttachmentVariable_output_between_7V_and_10V_0BA8.Standard.lsc.zip (120 Downloads) |
Follow us on