3/20/2018 6:21 PM | |
Posts: 4 Rating: (0) |
In the past few days i'm trying to use the following miniPCIe board but without success. https://techship.com/products/option-gtm671wfs/# The module powers up and responds to AT commands but the sim card is not recognized. Anyone know where the miniPCIe header in the IOT2040 is connected to? More precisely the pins 16 UIM_VPP,14 UIM_RESET, 12 UIM_CLK, 10 UIM_DATA and 8 UIM_PWR as explaned in https://support.industry.siemens.com/cs/ww/en/view/109741658 section 7.5.3.3 Mini PCIe interface. Thank you, Nuno |
Last edited by: nuno407 at: 3/20/2018 6:51:34 PMLast edited by: Jen_Moderator at: 3/23/2018 7:51:09 AMOptimized link. |
|
3/22/2018 11:13 AM | |
Joined: 4/28/2015 Last visit: 11/12/2024 Posts: 3345 Rating: (379)
|
Hi, it looks like the UIM interface can't be used on the IOT, because it is not supported on the hardware. You have to use either a "mPCIe module with integrated SIM Card" or a "mPCIe module with SIM Card Connector". For this there are some Telit cards. Best regards! |
Not working for IOT2050 support anymore from March 1st, 2024. |
|
7/4/2018 4:20 PM | |
Joined: 4/28/2015 Last visit: 11/12/2024 Posts: 3345 Rating: (379)
|
Hi, there is a description how to use the Telit HE-910 D on github. Looks like he made his own image, but there is also a link in the history where you can find the kernel modules to activate. Best regards! |
Not working for IOT2050 support anymore from March 1st, 2024. |
|
10/25/2018 3:35 PM | |
Posts: 7 Rating: (2) |
Ralink RT5572 based Wifi USB Adapter works fine! Product example: CSL 300Mbit USB WLAN |
This contribution was helpful to2 thankful Users |
12/17/2018 11:57 AM | |
Joined: 4/28/2015 Last visit: 2/1/2023 Posts: 8 Rating: (0) |
Hello, does anyone know a WLAN stick the Plap & Play works with 5GHZ? |
12/17/2018 11:58 AM | |
Joined: 4/28/2015 Last visit: 2/1/2023 Posts: 8 Rating: (0) |
Plug&Play / no additional drivers needed ? |
12/17/2018 11:59 AM | |
Joined: 4/28/2015 Last visit: 2/1/2023 Posts: 8 Rating: (0) |
Plag and play or install the Driver? |
Follow us on