8/7/2006 11:11 PM | |
Posts: 3 Rating:
|
Hi, Is there any problem when you are using PLC's Thanks in advance. |
8/8/2006 9:18 AM | |
Joined: 4/24/2006 Last visit: 7/31/2025 Posts: 9027 Rating:
|
Hello Giorikas, The ordernr.: CPU 226 AC/DC/Relay 24I/16O---6ES7 216-2BD23-OXBO is the newest version. There are minor changes compare to the CPU 226 AC/DC/Relay 24I/16O---6ES7 216-2BD22-OXBO See following link: http://support.automation.siemens.com/WW/view/en/19168619 It's possible to use both CPU's in one project, that's no problem. Only the 'old' cpu doesn't have the new aspects. Hope this will help. Best regard, Wizard |
Follow us on