(0)| 5/1/2022 5:34 AM | |
|
Joined: 5/14/2021 Last visit: 11/12/2025 Posts: 1 Rating:
|
In one project we are facing problem with the FM 458-1 DP The hardware configuration is as below (see enclosed file):
a. ISO protocol through CP 443-1 b. PC adaptor (MPI) But the FM module is always in Stop mode.Stop LED is flashing.And when we go online in the HW config it shows themodule is not available. And also when we try to download the charts to FM the message we get is module not available. In the mean time to ascertain the problem we have tried the following without success:
We are not clear from the FM458-1 manuals about the following queries: Mishra ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 05/02/2022 11:43:56New subject after splitting |
|
| 5/2/2022 12:39 PM | |
|
Joined: 8/31/2005 Last visit: 12/16/2025 Posts: 2198 Rating:
|
The manual says at the end of section 2.1.6 a flashing STOP-LED means: Download running in the STOP condition. If possible, download the program offline into the MMC using a PG or the SIMATIC USB-Prommer. The online download via back plane may run only with 187,5 Mbit/s and you have to transfer up to 2MB ! As far as I know, you always have to use D7-SYS, CFC in the same main version, e.g. V6. I think D7-SYS in V6 and CFC in V7 is not working. |
Last edited by: miami at: 05/02/2022 12:42:17 |
|
Follow us on