(0)| 11/30/2023 10:32 AM | |
|
Posts: 6 Rating:
|
Dear Friend I got error like this. My system includes a S7-400 and ET200 CPU. In that ET200 there are some analog input modules (6ES7331-7PF11-0AB0), the system works normally. At that time, the production line was down for maintenance and an incident occurred that day. The first module has a flashing SF light. Then about 4 hours later, 2 more modules also encountered the SF flashing error. When checking the signal, interference was detected for a period of 2 hours and then the signal was lost. When checking the channels of the module, the voltage in the channels of the module is close to zero. I want to know the possible cause of signal noise and module failure. Thank you. I sent more pictures. everyone please help AttachmentImages.zip (565 Downloads) |
Last edited by: Jen_Moderator at: 12/01/2023 07:56:20All files added as .zip file. Last edited by: Jen_Moderator at: 12/01/2023 07:58:57Text formatting optimized. |
|
Follow us on